<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Should I use an external resistor to pull up the boot pin?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617543#M36839</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the KL03 and I'll unset the&amp;nbsp;BOOTPIN_OPT flag of the&amp;nbsp;FTFA_FOPT register. I'd like to make&amp;nbsp;the&amp;nbsp;user able to short GND and the boot pin during reset to trigger the bootloader as a safety firmware upgrade method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is whether I need to use a pull-up resistor for the boot pin, or is&amp;nbsp;the internal pull-up sufficient.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;- Laci&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Apr 2017 22:47:49 GMT</pubDate>
    <dc:creator>laszlomonda</dc:creator>
    <dc:date>2017-04-17T22:47:49Z</dc:date>
    <item>
      <title>Should I use an external resistor to pull up the boot pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617543#M36839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the KL03 and I'll unset the&amp;nbsp;BOOTPIN_OPT flag of the&amp;nbsp;FTFA_FOPT register. I'd like to make&amp;nbsp;the&amp;nbsp;user able to short GND and the boot pin during reset to trigger the bootloader as a safety firmware upgrade method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is whether I need to use a pull-up resistor for the boot pin, or is&amp;nbsp;the internal pull-up sufficient.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;- Laci&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 22:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617543#M36839</guid>
      <dc:creator>laszlomonda</dc:creator>
      <dc:date>2017-04-17T22:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: Should I use an external resistor to pull up the boot pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617544#M36840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Laci,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Please take care, the BOOTCFG0 pin is also the /NMI pin, from the /NMI pin recommend design, it is better to add the external 4.7K to 10K pull up resistor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;A class="link-titled" href="http://cache.nxp.com/assets/documents/data/en/user-guides/KLQRUG.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.nxp.com/assets/documents/data/en/user-guides/KLQRUG.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.nxp.com/assets/documents/data/en/user-guides/KLQRUG.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Page 23, chapter 2.1.3.4.1 RESET_b and NMI_b.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The MCU can work if you don't add the external pull up, but for good design, I suggest you to add the external 4.7k to 10K pull up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 01:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617544#M36840</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-04-19T01:40:27Z</dc:date>
    </item>
    <item>
      <title>Re: Should I use an external resistor to pull up the boot pin?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617545#M36841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Got it! Thank you, Kerry!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Apr 2017 00:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Should-I-use-an-external-resistor-to-pull-up-the-boot-pin/m-p/617545#M36841</guid>
      <dc:creator>laszlomonda</dc:creator>
      <dc:date>2017-04-27T00:32:33Z</dc:date>
    </item>
  </channel>
</rss>