<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: The connection between K64F output and 74LS07 input is OK? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-connection-between-K64F-output-and-74LS07-input-is-OK/m-p/617338#M36812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Masakazu Notsu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All 5V dital I/O are clamped to VSS through a protection diode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to K64's datasheet, chapter&amp;nbsp;2.2.1 Voltage and current operating requirements for more information:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Apr 2017 22:10:49 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2017-04-20T22:10:49Z</dc:date>
    <item>
      <title>The connection between K64F output and 74LS07 input is OK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-connection-between-K64F-output-and-74LS07-input-is-OK/m-p/617337#M36811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kinetis K64F output pins are connecting to input pins of SN74LS07 buffer.&lt;/P&gt;&lt;P&gt;The Vcc of SN74LS07 is 5V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works normally.&lt;/P&gt;&lt;P&gt;However, I am worried about the reverse current to K64F Vdd (3.3V) from SN74LS07 input pin.&lt;BR /&gt;SN74LS07 datasheet says "I_IH is 20uA, I_IL is -0.2mA".&lt;/P&gt;&lt;P&gt;Are these value no problem for K64F ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I had thought that All digital I/O pins are 5V tolerant.&lt;BR /&gt;But some people say that "The Kinetis Port pins are only 5V tolerant as inputs. The outputs are not 5V tolerant." in other threads.&lt;BR /&gt;Which is true?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 03:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-connection-between-K64F-output-and-74LS07-input-is-OK/m-p/617337#M36811</guid>
      <dc:creator>masakazunotsu</dc:creator>
      <dc:date>2017-04-18T03:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: The connection between K64F output and 74LS07 input is OK?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-connection-between-K64F-output-and-74LS07-input-is-OK/m-p/617338#M36812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Masakazu Notsu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All 5V dital I/O are clamped to VSS through a protection diode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to K64's datasheet, chapter&amp;nbsp;2.2.1 Voltage and current operating requirements for more information:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/data_sheet/K64P144M120SF5.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Apr 2017 22:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-connection-between-K64F-output-and-74LS07-input-is-OK/m-p/617338#M36812</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2017-04-20T22:10:49Z</dc:date>
    </item>
  </channel>
</rss>