<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB CCID Communication Problem in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CCID-Communication-Problem/m-p/616930#M36770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am&amp;nbsp;developing an application in which the FRDM-K82F will transfer data to the front end software using USB CCID command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I successfully convert the USB-CCID code from K64(&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;K64 USB CCID demo.&lt;/SPAN&gt;) to K82, and the windows recognized the K82 board as "Microsoft USBCCID smart card reader".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;windows is sending GET_SLOTSTATUS command and K82 reply to this command. After this windows is sending ICC_POWERON command and the K82 reply to this command also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the windows is sending ICC_POWEROFF command and the K82 reply to it, &amp;nbsp;(after that the process is in loop like POWERON , POWEROFF). I am unable to proceed any data communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please anyone help me to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mohammad Gouse&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Oct 2016 11:48:24 GMT</pubDate>
    <dc:creator>gouse_saudi</dc:creator>
    <dc:date>2016-10-31T11:48:24Z</dc:date>
    <item>
      <title>USB CCID Communication Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CCID-Communication-Problem/m-p/616930#M36770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am&amp;nbsp;developing an application in which the FRDM-K82F will transfer data to the front end software using USB CCID command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I successfully convert the USB-CCID code from K64(&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;K64 USB CCID demo.&lt;/SPAN&gt;) to K82, and the windows recognized the K82 board as "Microsoft USBCCID smart card reader".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;windows is sending GET_SLOTSTATUS command and K82 reply to this command. After this windows is sending ICC_POWERON command and the K82 reply to this command also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then the windows is sending ICC_POWEROFF command and the K82 reply to it, &amp;nbsp;(after that the process is in loop like POWERON , POWEROFF). I am unable to proceed any data communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please anyone help me to solve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mohammad Gouse&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Oct 2016 11:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CCID-Communication-Problem/m-p/616930#M36770</guid>
      <dc:creator>gouse_saudi</dc:creator>
      <dc:date>2016-10-31T11:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB CCID Communication Problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CCID-Communication-Problem/m-p/616931#M36771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mohammad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K64's CCID project is using UART-ISO7816 to communciate with cards, however, K8x module has a EMV module which is specially designed to communicate with these cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For newest KSDK 2.1 version, there is an example for K80 MCU available at: &amp;lt;\SDK_2.1_TWR-K80F150M_PATH&amp;gt;\boards\twrk80f150m\usb_examples\usb_device_ccid_smart_card than can be used as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 21:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-CCID-Communication-Problem/m-p/616931#M36771</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-11-28T21:14:26Z</dc:date>
    </item>
  </channel>
</rss>