<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Please help me recommend a brushless DC motor development kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-help-me-recommend-a-brushless-DC-motor-development-kit/m-p/615117#M36579</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Simith,&lt;/P&gt;&lt;P&gt;Pls refer to the website for KEA family application to control BLDC.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/3-phase-sensorless-bldc-motor-control-reference-design-based-on-kinetis-kea128-mcus:KEA128BLDCRD" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/3-phase-sensorless-bldc-motor-control-reference-design-based-on-kinetis-kea128-mcus:KEA128BLDCRD"&gt;3-phase Sensorless BLDC Motor Control RD|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you use Hall sensor to detect position of rotor, as you know that the KEA has three FTM modules, FTM0 can be used to generate 3 pair PWM signals, FTM1 and FTM2 can be used to detect Hall signal with capture function so that rising/falling edges of three hall signals can be used to trigger interrupt, compute the speed. You can connect 3 hall signals to FTM1 or FTM2&amp;nbsp; channels for example FTM1_CHx, it is okay. For forward, reverse, speed regulation, it is dependent on software.&lt;/P&gt;&lt;P&gt;I think any KEA family is okay to control BLDC.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Dec 2016 08:20:05 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-12-16T08:20:05Z</dc:date>
    <item>
      <title>Please help me recommend a brushless DC motor development kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-help-me-recommend-a-brushless-DC-motor-development-kit/m-p/615116#M36578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please help me recommend a brushless DC motor development kit, that is, including the controller, procedures and motors.&lt;BR /&gt;Specific requirements:&lt;BR /&gt;1, the controller chip needs to be KEA128 or 64, if not， others are OK，but its performance and programming is closer to the KEA128;&lt;BR /&gt;2, the program needs to be for BLDC with position hall sensors;&lt;BR /&gt;3, the program needs to achieve forward, reverse, speed regulation , other basic functions and some commonly used algorithms;&lt;BR /&gt;4, driven motor and power circuit can be changed, the latter need to test the motor of different power levels;&lt;BR /&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 11:19:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-help-me-recommend-a-brushless-DC-motor-development-kit/m-p/615116#M36578</guid>
      <dc:creator>simithli</dc:creator>
      <dc:date>2016-12-15T11:19:16Z</dc:date>
    </item>
    <item>
      <title>Re: Please help me recommend a brushless DC motor development kit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-help-me-recommend-a-brushless-DC-motor-development-kit/m-p/615117#M36579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Simith,&lt;/P&gt;&lt;P&gt;Pls refer to the website for KEA family application to control BLDC.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/3-phase-sensorless-bldc-motor-control-reference-design-based-on-kinetis-kea128-mcus:KEA128BLDCRD" title="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/ea-series-automotive-m0-plus/3-phase-sensorless-bldc-motor-control-reference-design-based-on-kinetis-kea128-mcus:KEA128BLDCRD"&gt;3-phase Sensorless BLDC Motor Control RD|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you use Hall sensor to detect position of rotor, as you know that the KEA has three FTM modules, FTM0 can be used to generate 3 pair PWM signals, FTM1 and FTM2 can be used to detect Hall signal with capture function so that rising/falling edges of three hall signals can be used to trigger interrupt, compute the speed. You can connect 3 hall signals to FTM1 or FTM2&amp;nbsp; channels for example FTM1_CHx, it is okay. For forward, reverse, speed regulation, it is dependent on software.&lt;/P&gt;&lt;P&gt;I think any KEA family is okay to control BLDC.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 08:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Please-help-me-recommend-a-brushless-DC-motor-development-kit/m-p/615117#M36579</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-12-16T08:20:05Z</dc:date>
    </item>
  </channel>
</rss>