<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM64f UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614979#M36574</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you're using OpenSDA built in uart, you have to use B16 and B17 pins, in other modules you need to connect RX, TX,&amp;nbsp; GND. Remember also to set properly baud and enable both receiver and transmitter.&lt;/P&gt;&lt;P&gt;If you want to use interrupts, you need to enable "on receiver full" interrupt methode and in the main file create ISR function like PE_ISR(yourISRnameHERE){...} or let PE do that for you (project-&amp;gt;properties-&amp;gt;PE-&amp;gt;generate ISR).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Nov 2016 07:25:01 GMT</pubDate>
    <dc:creator>wojciechlesniew</dc:creator>
    <dc:date>2016-11-28T07:25:01Z</dc:date>
    <item>
      <title>FRDM64f UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614977#M36572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: 12.8px;"&gt;I'm using FRDM-64F board for my project.I need to get the UART receiving data whenever it arrives on receive pin.I used UART3 PTC16 and PTC17 pins for UART and KDS as IDE. I tried several interrupt configuration,which are not working .Using&amp;nbsp;UART_DRV_ReceiveData for reception which is also interrupt controlled that also not working.Please help me for solving that issue.Suggest any other pins, which is available on the board.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 13:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614977#M36572</guid>
      <dc:creator>ajaykr</dc:creator>
      <dc:date>2016-11-22T13:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM64f UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614978#M36573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check my colleague's comments at below thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/853791"&gt;https://community.nxp.com/message/853791 &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 09:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614978#M36573</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-11-25T09:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM64f UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614979#M36574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you're using OpenSDA built in uart, you have to use B16 and B17 pins, in other modules you need to connect RX, TX,&amp;nbsp; GND. Remember also to set properly baud and enable both receiver and transmitter.&lt;/P&gt;&lt;P&gt;If you want to use interrupts, you need to enable "on receiver full" interrupt methode and in the main file create ISR function like PE_ISR(yourISRnameHERE){...} or let PE do that for you (project-&amp;gt;properties-&amp;gt;PE-&amp;gt;generate ISR).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 07:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614979#M36574</guid>
      <dc:creator>wojciechlesniew</dc:creator>
      <dc:date>2016-11-28T07:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM64f UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614980#M36575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the support.I referenced the code of lwip HTTP server creation&lt;/P&gt;&lt;P&gt;in FRDM-64f.How can I receive data from webpage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Mon, Nov 28, 2016 at 12:55 PM, wojciechlesniewicz &amp;lt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 12:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM64f-UART/m-p/614980#M36575</guid>
      <dc:creator>ajaykr</dc:creator>
      <dc:date>2016-12-02T12:23:39Z</dc:date>
    </item>
  </channel>
</rss>