<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis KV10Z32xx7 self lock problems in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614147#M36446</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just found that J-Flash Lite erase function would case KV10Z32xx7 to secure himself. In this case, the mcus can be unsecure with following steps, found by myself:&lt;/P&gt;&lt;P&gt;1. Power off MCU&lt;BR /&gt;2. MCU rst pin (pin19) pull to ground&lt;BR /&gt;3. Power on mcu&lt;BR /&gt;4. J-link&amp;gt;Unlock Kinetis.&lt;BR /&gt;5. Flash a dummy binary or hex file(eg gpio example)&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;For those mcus securing themself not because of j-Flash Lite (still unknown for me), the above method is not applicable.&lt;/P&gt;&lt;P&gt;I still have no solution in the case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Apr 2017 07:31:03 GMT</pubDate>
    <dc:creator>zhitailiu</dc:creator>
    <dc:date>2017-04-18T07:31:03Z</dc:date>
    <item>
      <title>Kinetis KV10Z32xx7 self lock problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614146#M36445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, first time design with NXP/Fressscale mcu. In the beginning, I use FRDM KV10Z to develop firmware, it goes pretty well. However, when I first time using my custom PCB with 32 pin LQFP kv10Z32vlc7, sometime the mcu locks himself accidentally! I am using J-Link and KEIL uVsition. Sometime it goes well, but very often my Jlink&amp;nbsp;cannot connect with the mcu and having the following msg:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6730i1A3D8C826EEFB66C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Once jLink shows these message, I cannot unsecure this mcu anymore, I have to desolder it and replace by a new one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried about 10 pcs, now there are 4 of them got locked!&lt;/P&gt;&lt;P&gt;Please help me here. I've spent few days on this, and getting frustrating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE:&lt;/P&gt;&lt;P&gt;1 Jlink is connected to MCU through SWD_CLK, SWD_IO, Gnd, VCC. Reset_b pin and NMI_b pins are pulled high externally.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2 I noticed that when the reset_b pin is not pulled high (left open), it goes low by itself. This is quit strange.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Apr 2017 10:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614146#M36445</guid>
      <dc:creator>zhitailiu</dc:creator>
      <dc:date>2017-04-17T10:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KV10Z32xx7 self lock problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614147#M36446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just found that J-Flash Lite erase function would case KV10Z32xx7 to secure himself. In this case, the mcus can be unsecure with following steps, found by myself:&lt;/P&gt;&lt;P&gt;1. Power off MCU&lt;BR /&gt;2. MCU rst pin (pin19) pull to ground&lt;BR /&gt;3. Power on mcu&lt;BR /&gt;4. J-link&amp;gt;Unlock Kinetis.&lt;BR /&gt;5. Flash a dummy binary or hex file(eg gpio example)&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;For those mcus securing themself not because of j-Flash Lite (still unknown for me), the above method is not applicable.&lt;/P&gt;&lt;P&gt;I still have no solution in the case.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Apr 2017 07:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614147#M36446</guid>
      <dc:creator>zhitailiu</dc:creator>
      <dc:date>2017-04-18T07:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KV10Z32xx7 self lock problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614148#M36447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a document about Kinetis Lock and how to unlock the Kinetis chip.&lt;/P&gt;&lt;P&gt;More detailed info, please check below link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329424"&gt;https://community.nxp.com/docs/DOC-329424&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Apr 2017 02:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KV10Z32xx7-self-lock-problems/m-p/614148#M36447</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-04-19T02:28:54Z</dc:date>
    </item>
  </channel>
</rss>