<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Power supply for KL82</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614130#M36444</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet page125 indicated VDDIO_E voltage range, which should be greater than or equal to VDD voltage.&lt;/P&gt;&lt;P&gt;The related info also was showed at datasheet table41:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15319i6EB54476CBDE17B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In fact, just using FRDM-KL82Z board as an example:&lt;/P&gt;&lt;P&gt;If VDD was powered with 1.8V, the VDDIO_E voltage can't be powered with 1.8V. For external QSPI Flash powered with 3.3V,&amp;nbsp; VDDIO_E need be powered with 3.3V. VDDIO_E voltage is greater than VDD voltage.&lt;/P&gt;&lt;P&gt;If VDD was powered with 3.3V, the VDDIO_E voltage is same with VDD voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet page68 shows the two voltage (VDDIO/VDD) power up sequence and power down sequence.&lt;/P&gt;&lt;P&gt;There with requirement: VDDIO must never be higher than VDD during power ramp up, or power down.&lt;/P&gt;&lt;P&gt;If VDD was powered with 1.8V and VDDIO_E was powered with 3.3V, there with requirement that: during 0~1.8V power ramp up, the VDDIO_E voltage couldn't higher than&amp;nbsp; VDD. After VDD reach 1.8V, there without this restriction.&lt;/P&gt;&lt;P&gt;If VDD and VDDIO_E were powered with 3.3V, tie VDD and VDDIO to the same power supply is a reasonable choice.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Mar 2017 08:40:12 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-03-03T08:40:12Z</dc:date>
    <item>
      <title>Power supply for KL82</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614127#M36441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am going to make a customer board with kl82. I have question about kl82 power supply. In Page 125 of datasheet, it says: • VDDIO_E, which is dedicated to powering PORTE, must be powered after VDD and must be greater than or equal to VDD voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While in page 62, it says&amp;nbsp;&lt;/P&gt;&lt;P&gt;VDDIO is independent of VDD domain and can operate at a voltage independent of VDD. However, it is required that VDD&lt;BR /&gt;domain be powered up first prior to VDDIO. VDDIO must never be higher than VDD during power ramp up, or power down.&lt;BR /&gt;VDD and VDDIO may ramp together if tied to the same power supply.&lt;/P&gt;&lt;P&gt;VDDIO is an independent voltage supply for PORTE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am confused by those two power up requirement. Is it possible for NXP&amp;nbsp;to clarify this point?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bo Peng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 11:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614127#M36441</guid>
      <dc:creator>bopeng</dc:creator>
      <dc:date>2017-03-02T11:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply for KL82</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614128#M36442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VDDIO pin provide power to PORT E pins.&lt;/P&gt;&lt;P&gt;PORTE pins has QuadSPI feature to access QSPI flash.&lt;/P&gt;&lt;P&gt;FRDM-KL82Z board hardware design file could be downloaded from &lt;A href="http://www.nxp.com/assets/downloads/data/en/printed-circuit-boards/FRDM-KL82Z.zip"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Please refer FRDM-KL82Z schematics for the detailed circuit design.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 07:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614128#M36442</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-03-03T07:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply for KL82</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614129#M36443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have checked the schematic. But it is different with the requirement with Datasheet. And the datasheet has two different requirements. I want to make sure from NXP which one is correct way.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 07:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614129#M36443</guid>
      <dc:creator>bopeng</dc:creator>
      <dc:date>2017-03-03T07:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: Power supply for KL82</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614130#M36444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet page125 indicated VDDIO_E voltage range, which should be greater than or equal to VDD voltage.&lt;/P&gt;&lt;P&gt;The related info also was showed at datasheet table41:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15319i6EB54476CBDE17B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In fact, just using FRDM-KL82Z board as an example:&lt;/P&gt;&lt;P&gt;If VDD was powered with 1.8V, the VDDIO_E voltage can't be powered with 1.8V. For external QSPI Flash powered with 3.3V,&amp;nbsp; VDDIO_E need be powered with 3.3V. VDDIO_E voltage is greater than VDD voltage.&lt;/P&gt;&lt;P&gt;If VDD was powered with 3.3V, the VDDIO_E voltage is same with VDD voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet page68 shows the two voltage (VDDIO/VDD) power up sequence and power down sequence.&lt;/P&gt;&lt;P&gt;There with requirement: VDDIO must never be higher than VDD during power ramp up, or power down.&lt;/P&gt;&lt;P&gt;If VDD was powered with 1.8V and VDDIO_E was powered with 3.3V, there with requirement that: during 0~1.8V power ramp up, the VDDIO_E voltage couldn't higher than&amp;nbsp; VDD. After VDD reach 1.8V, there without this restriction.&lt;/P&gt;&lt;P&gt;If VDD and VDDIO_E were powered with 3.3V, tie VDD and VDDIO to the same power supply is a reasonable choice.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Mar 2017 08:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Power-supply-for-KL82/m-p/614130#M36444</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-03-03T08:40:12Z</dc:date>
    </item>
  </channel>
</rss>