<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Recommendations for Complete Toolchain</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214132#M3641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;jbd,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CodeWarrior is certainly a good option. &amp;nbsp;The code-size limited version (Special Edition) is free. You can try out the full version with the 30-day license that comes with it and you can go into your license account on freescale.com and automatically up it to a 90-day license if needed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale MQX RTOS is a complimentary solution with a comprehensive USB stack. &amp;nbsp;Also check out the stand-alone USB stack from Freescale. &amp;nbsp;It is (poorly) named "﻿﻿USB Stack with PHDC Support". &amp;nbsp;Kinetis support was introduced in version 3.0 and the class support is quite comprehensive. &amp;nbsp;Check it out here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached the readme.txt file which contains the release notes so you can see what is currently supported for Kinetis and what isn't.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-mnorman&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jun 2011 22:43:27 GMT</pubDate>
    <dc:creator>mnorman</dc:creator>
    <dc:date>2011-06-10T22:43:27Z</dc:date>
    <item>
      <title>Recommendations for Complete Toolchain</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214131#M3640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does anyone have any recomendations on a toolchain (IDE + Compiler + RTOS + Debug Tool) for the Kinetis processors that they are happy with? &amp;nbsp;I plan to work on a custom board. &amp;nbsp;Something that I could get started with for cheap and then pay more later as I need more capability would be preferred. &amp;nbsp;Codewarrior and CodeSourcery are pretty appealing there. &amp;nbsp;And of course something that is easy to get started with would also be good. &amp;nbsp;I don't need a TCPiP stack, but I do need USB Device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;JD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2011 21:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214131#M3640</guid>
      <dc:creator>jbd</dc:creator>
      <dc:date>2011-06-10T21:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: Recommendations for Complete Toolchain</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214132#M3641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;jbd,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CodeWarrior is certainly a good option. &amp;nbsp;The code-size limited version (Special Edition) is free. You can try out the full version with the 30-day license that comes with it and you can go into your license account on freescale.com and automatically up it to a 90-day license if needed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale MQX RTOS is a complimentary solution with a comprehensive USB stack. &amp;nbsp;Also check out the stand-alone USB stack from Freescale. &amp;nbsp;It is (poorly) named "﻿﻿USB Stack with PHDC Support". &amp;nbsp;Kinetis support was introduced in version 3.0 and the class support is quite comprehensive. &amp;nbsp;Check it out here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've attached the readme.txt file which contains the release notes so you can see what is currently supported for Kinetis and what isn't.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-mnorman&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2011 22:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214132#M3641</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2011-06-10T22:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: Recommendations for Complete Toolchain</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214133#M3642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks mnormam.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Assuming that I go with Code Warrior and MQX, what debug tool would you suggest that integrates easily with CW? &amp;nbsp;And if I wanted trace capability (probably not needed initially), what tool then?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-jbd&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jun 2011 03:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214133#M3642</guid>
      <dc:creator>jbd</dc:creator>
      <dc:date>2011-06-11T03:52:31Z</dc:date>
    </item>
    <item>
      <title>Re: Recommendations for Complete Toolchain</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214134#M3643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The uTasker project also includes USB device support for the Kinetis (CDC - &lt;EM&gt;the most popular communication class&lt;/EM&gt; - and MSD).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Its project includes compiler builds for CW10.1, IAR6, uVision4, GCC and Rowley Crossworks V2.1 so is essentially tool-independent.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It includes a real-time Kinetis simulator for more efficient development - allowing development and test in VisualStudio environment (USB is an exception since it can't be simulated directly but can still be used for development and verification using simulation scripts).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;More details in this forum here: &lt;A __default_attr="77616" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/77616" jivemacro="thread" title="https://community.freescale.com/thread/77616"&gt;https://community.freescale.com/thread/77616&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jun 2011 20:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Recommendations-for-Complete-Toolchain/m-p/214134#M3643</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-06-11T20:20:56Z</dc:date>
    </item>
  </channel>
</rss>