<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KEA8 internal temperature sensor</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613467#M36370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to use the internal temperature sensor, I'm using kea8 kinetis microcontroller.&lt;/P&gt;&lt;P&gt;When I sample an ordinary analog input, from external pin, it is all right, but when I try to sample an internal analog channel (Vbandgap or temperature sensor) the value that I have obtained is not consistent, very unstable and change if I start the conversion mode. For example, starting the bandgap sampling by:&lt;/P&gt;&lt;P&gt;ADC_SC1 &amp;amp;= ~0x0000001f;&lt;/P&gt;&lt;P&gt;ADC_SC1 |= 23;&amp;nbsp;&amp;nbsp; // sampling bandgap channel&lt;/P&gt;&lt;P&gt;obtain the result from about 0x300 to 0xaff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;elsewhere by setting&lt;/P&gt;&lt;P&gt;ACD_SC1 = 23 | INTERRUPT_ENABLE_MASK;&lt;/P&gt;&lt;P&gt;the result is from 0x100 to 0x12f;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC is configured for long sample time and with different clock frequency (busclock = 5 to 20 MHz, ADCLK = busclock /4 to 16).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion to solve my problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jan 2017 09:37:32 GMT</pubDate>
    <dc:creator>alessiodemarchi</dc:creator>
    <dc:date>2017-01-13T09:37:32Z</dc:date>
    <item>
      <title>KEA8 internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613467#M36370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try to use the internal temperature sensor, I'm using kea8 kinetis microcontroller.&lt;/P&gt;&lt;P&gt;When I sample an ordinary analog input, from external pin, it is all right, but when I try to sample an internal analog channel (Vbandgap or temperature sensor) the value that I have obtained is not consistent, very unstable and change if I start the conversion mode. For example, starting the bandgap sampling by:&lt;/P&gt;&lt;P&gt;ADC_SC1 &amp;amp;= ~0x0000001f;&lt;/P&gt;&lt;P&gt;ADC_SC1 |= 23;&amp;nbsp;&amp;nbsp; // sampling bandgap channel&lt;/P&gt;&lt;P&gt;obtain the result from about 0x300 to 0xaff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;elsewhere by setting&lt;/P&gt;&lt;P&gt;ACD_SC1 = 23 | INTERRUPT_ENABLE_MASK;&lt;/P&gt;&lt;P&gt;the result is from 0x100 to 0x12f;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC is configured for long sample time and with different clock frequency (busclock = 5 to 20 MHz, ADCLK = busclock /4 to 16).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion to solve my problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 09:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613467#M36370</guid>
      <dc:creator>alessiodemarchi</dc:creator>
      <dc:date>2017-01-13T09:37:32Z</dc:date>
    </item>
    <item>
      <title>Re: KEA8 internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613468#M36371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="290944" data-username="alessiodemarchi" href="https://community.nxp.com/people/alessiodemarchi"&gt;Alessio De Marchi&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I apologize for this delay, please check this &lt;A href="http://cache.nxp.com/assets/documents/data/en/application-notes/AN3031.pdf?fsrch=1&amp;amp;sr=4&amp;amp;pageNum=1"&gt;Application note&lt;/A&gt;, it is for 8bit but &amp;nbsp;the process is the same &amp;nbsp;hope this help you solve your problem.&lt;/P&gt;&lt;P&gt;have a great day !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 17:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613468#M36371</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2017-02-15T17:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: KEA8 internal temperature sensor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613469#M36372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't especially help with your 'inconsistent ADC reads' -- you will certainly need to solve THAT!&amp;nbsp; (Did you enable the bandgap device?).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But as for AN3031, I highly recommend my more comprehensive post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/390524"&gt;On-chip temperature Calculations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 17:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA8-internal-temperature-sensor/m-p/613469#M36372</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-02-15T17:36:09Z</dc:date>
    </item>
  </channel>
</rss>