<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flow control of UART for FRDM-KL43Z in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flow-control-of-UART-for-FRDM-KL43Z/m-p/613189#M36347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi expert,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just two simple questions(Platform FRDM-KL43Z, board: MKL43Z256xxx4, SDK 2, KDS: 3.2.0):&lt;/P&gt;&lt;P&gt;1) Does this platform support hardware control (RTS/PTS) for UART? I can see that the MKL43Z4_features.h define the&amp;nbsp;FSL_FEATURE_UART_HAS_MODEM_SUPPORT to 0. So this platform does not support hardware flow control, right?&lt;/P&gt;&lt;P&gt;2) Can I realise a UART with hardware control with FLEXio??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Kaikai&lt;/P&gt;&lt;P&gt;Blue Creation, Cambridge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 16:06:36 GMT</pubDate>
    <dc:creator>kaikailiu</dc:creator>
    <dc:date>2016-12-14T16:06:36Z</dc:date>
    <item>
      <title>Flow control of UART for FRDM-KL43Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flow-control-of-UART-for-FRDM-KL43Z/m-p/613189#M36347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi expert,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just two simple questions(Platform FRDM-KL43Z, board: MKL43Z256xxx4, SDK 2, KDS: 3.2.0):&lt;/P&gt;&lt;P&gt;1) Does this platform support hardware control (RTS/PTS) for UART? I can see that the MKL43Z4_features.h define the&amp;nbsp;FSL_FEATURE_UART_HAS_MODEM_SUPPORT to 0. So this platform does not support hardware flow control, right?&lt;/P&gt;&lt;P&gt;2) Can I realise a UART with hardware control with FLEXio??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Kaikai&lt;/P&gt;&lt;P&gt;Blue Creation, Cambridge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 16:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flow-control-of-UART-for-FRDM-KL43Z/m-p/613189#M36347</guid>
      <dc:creator>kaikailiu</dc:creator>
      <dc:date>2016-12-14T16:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: Flow control of UART for FRDM-KL43Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flow-control-of-UART-for-FRDM-KL43Z/m-p/613190#M36348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kaikai,&lt;BR /&gt;1) The UART and LPUART module of KL43 doesn't support support hardware flow control (RTS/CTS).&lt;/P&gt;&lt;P&gt;2) The FlexIO module can be used to realize UART hardware flow control (RTS/CTS). For more detail please read the section "39.5.1 UART Transmit" and "39.5.2 UART Receive" in &lt;A href="http://www.nxp.com/assets/documents/data/en/reference-manuals/KL43P64M48SF6RM.pdf"&gt;KL43P64M48SF6RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2016 01:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flow-control-of-UART-for-FRDM-KL43Z/m-p/613190#M36348</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-12-16T01:41:48Z</dc:date>
    </item>
  </channel>
</rss>