<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MKM34 Reference voltage</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-Reference-voltage/m-p/612686#M36309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Druv,&lt;/P&gt;&lt;P&gt;software setting looks correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that when internal 1.2 V VREF is routed through VREF buffer&amp;nbsp;out to VREF pin, then 100 nF capacitor&amp;nbsp;must be connected between VREF&amp;nbsp;and GNDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Martin M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Apr 2017 21:01:14 GMT</pubDate>
    <dc:creator>MarMi</dc:creator>
    <dc:date>2017-04-14T21:01:14Z</dc:date>
    <item>
      <title>MKM34 Reference voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-Reference-voltage/m-p/612685#M36308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have configured the device in the Internal Reference Mode. I am using MKM34Z256VLQ7.&lt;/P&gt;&lt;P&gt;I am not getting the 1.2V on VREF Pin. But I am getting 1.2 V on VREFH pin. Here is the Code for reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void main()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;SMC_Init (SMC_MODULE_VLPS_ON_VLLS_ON_CONFIG);&lt;BR /&gt;/* initialize SIM module */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM_Init (SIM_MODULE_NORM_MODE_SYSCLKMODE_SYSCLK_DIV1_CONFIG);&lt;/P&gt;&lt;P&gt;SIM_SelClkout (CLKOUT_SRC1);&lt;BR /&gt;PORT_Init (PORTF,PORT_MODULE_ALT3_MODE,PIN7);&lt;/P&gt;&lt;P&gt;/* clock mode 2:1:1, 48MHz */&lt;BR /&gt;SIM_SetClkMode (SYSCLK_MODE1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM_SetClkDiv (SYSCLK_DIV1);&lt;BR /&gt;FLL_Init (FLL_MODULE_FEE_48MHZ_CONFIG);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* sets 32 kHz RTC Oscillator as the source of the PLL and enable PLL */&lt;BR /&gt;PLL_Enable (PLL32KREF_SRC1);&lt;/P&gt;&lt;P&gt;/* VREF module must be initialized after SIM module */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VREF_Init (VREF_MODULE_CHOP_ON_1V75_0V4_HPWR_CONFIG,&lt;BR /&gt;VREF_SWITCH_S1_H_S2_L_S3_L_BUFF_EN);&lt;BR /&gt; &lt;BR /&gt;VREFL_Trim( 3); /* VREFL trimmed to 0.400 V */&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/***************************************************************************//*!&lt;BR /&gt;* @brief Voltage reference switch setting.&lt;BR /&gt;* @details Configures voltage reference switches:&lt;BR /&gt;* - Buffer enable,&lt;BR /&gt;* - Buffer drive voltage on PAD, S1 = H,&lt;BR /&gt;* - Internal reference select, S2 = L,&lt;BR /&gt;* - AFE Internal reference select, S3 = L,&lt;BR /&gt;* @showinitializer&lt;BR /&gt;******************************************************************************/&lt;BR /&gt;#define VREF_SWITCH_S1_H_S2_L_S3_L_BUFF_EN \&lt;BR /&gt;(tVREF_S){ \&lt;BR /&gt;/* SIM_MISC */ CLR(SIM_MISC_CTL_VREFBUFPD_MASK)| \&lt;BR /&gt;/* ......... */ CLR(SIM_MISC_CTL_VREFBUFINSEL_MASK)| \&lt;BR /&gt;/* ......... */ SET(SIM_MISC_CTL_VREFBUFOUTEN_MASK), \&lt;BR /&gt;/* VERFL_TRM */ CLR(VREF_VREFL_TRM_VREFL_SEL_MASK), \&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dhruv&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2017 11:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-Reference-voltage/m-p/612685#M36308</guid>
      <dc:creator>dhruvonline</dc:creator>
      <dc:date>2017-04-14T11:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: MKM34 Reference voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-Reference-voltage/m-p/612686#M36309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Druv,&lt;/P&gt;&lt;P&gt;software setting looks correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that when internal 1.2 V VREF is routed through VREF buffer&amp;nbsp;out to VREF pin, then 100 nF capacitor&amp;nbsp;must be connected between VREF&amp;nbsp;and GNDA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Martin M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2017 21:01:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKM34-Reference-voltage/m-p/612686#M36309</guid>
      <dc:creator>MarMi</dc:creator>
      <dc:date>2017-04-14T21:01:14Z</dc:date>
    </item>
  </channel>
</rss>