<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K61 DDR2 Max Frequency in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-DDR2-Max-Frequency/m-p/612381#M36280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="296522" data-username="mosheyotam" href="https://community.nxp.com/people/mosheyotam"&gt;Moshe Yotam&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I think this is an error in the RM, you can use the DDR as 150Mhz or less.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Mar 2017 20:08:53 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2017-03-27T20:08:53Z</dc:date>
    <item>
      <title>K61 DDR2 Max Frequency</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-DDR2-Max-Frequency/m-p/612380#M36279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, The following section is taken from the K61 reference manual&amp;nbsp;K61P256M150SF3RM.&lt;/P&gt;&lt;P&gt;Per #4: 'The DDR clock must be less than 150 MHz' &amp;nbsp;is that means it cannot run at 150 MHz ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16634i64A601C9D977CB44/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 09:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-DDR2-Max-Frequency/m-p/612380#M36279</guid>
      <dc:creator>mosheyotam</dc:creator>
      <dc:date>2017-03-23T09:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: K61 DDR2 Max Frequency</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-DDR2-Max-Frequency/m-p/612381#M36280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="296522" data-username="mosheyotam" href="https://community.nxp.com/people/mosheyotam"&gt;Moshe Yotam&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I think this is an error in the RM, you can use the DDR as 150Mhz or less.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 20:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-DDR2-Max-Frequency/m-p/612381#M36280</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2017-03-27T20:08:53Z</dc:date>
    </item>
  </channel>
</rss>