<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWatchdog timer in K22FN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612371#M36276</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just a simple question, how can I calculate the&amp;nbsp;timer value for the watchdog in K22?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the API, I can see that by default uses the LPO clock, which is rated as 1KHz. The timeout value from the wdog_config_t struct is&amp;nbsp;uint32_t so it can hold up to 0xFFFFFFFFU, or&amp;nbsp;‭4294967295‬ cycles. The reference manual does not seem to limit the value to something lower than that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean that the maximum possible value for the watchdog is&amp;nbsp;&lt;SPAN&gt;‭4294967 seconds?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If so, from the API documentation, the default value is 0xFFFFU, meaning a default watchdog value of 65 seconds. Is that&amp;nbsp;correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jan 2017 19:03:40 GMT</pubDate>
    <dc:creator>thiagopalmieri</dc:creator>
    <dc:date>2017-01-12T19:03:40Z</dc:date>
    <item>
      <title>Watchdog timer in K22FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612371#M36276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just a simple question, how can I calculate the&amp;nbsp;timer value for the watchdog in K22?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the API, I can see that by default uses the LPO clock, which is rated as 1KHz. The timeout value from the wdog_config_t struct is&amp;nbsp;uint32_t so it can hold up to 0xFFFFFFFFU, or&amp;nbsp;‭4294967295‬ cycles. The reference manual does not seem to limit the value to something lower than that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean that the maximum possible value for the watchdog is&amp;nbsp;&lt;SPAN&gt;‭4294967 seconds?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If so, from the API documentation, the default value is 0xFFFFU, meaning a default watchdog value of 65 seconds. Is that&amp;nbsp;correct?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 19:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612371#M36276</guid>
      <dc:creator>thiagopalmieri</dc:creator>
      <dc:date>2017-01-12T19:03:40Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog timer in K22FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612372#M36277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Thiago,&lt;/P&gt;&lt;P&gt;There is a 3-bit prescaler(WDOG_PRESC) for the watchdog clock source. So you need take it into account.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11482i3D8E39317E4A6645/image-size/large?v=v2&amp;amp;px=999" title="WDOG_PRESC.png" alt="WDOG_PRESC.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 08:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612372#M36277</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-01-13T08:07:57Z</dc:date>
    </item>
    <item>
      <title>Re: Watchdog timer in K22FN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612373#M36278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, so considering a prescaler of 1, putting 3000 into the timeout value, will give me a 3 second watchdog.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 00:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Watchdog-timer-in-K22FN/m-p/612373#M36278</guid>
      <dc:creator>thiagopalmieri</dc:creator>
      <dc:date>2017-01-16T00:47:00Z</dc:date>
    </item>
  </channel>
</rss>