<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Contradiction in reference manual K02P64M100SFARM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612308#M36268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So i can use a 25MHz crystal without external capacitors and without external resistor?&lt;/P&gt;&lt;P&gt;Is this a reliable solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Nov 2016 09:36:51 GMT</pubDate>
    <dc:creator>johnsmith3</dc:creator>
    <dc:date>2016-11-25T09:36:51Z</dc:date>
    <item>
      <title>Contradiction in reference manual K02P64M100SFARM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612306#M36266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a&amp;nbsp;MK02FN64VFM10 and want to use a 25 MHz external crystal.&lt;/P&gt;&lt;P&gt;In reference manual&amp;nbsp;K02P64M100SFARM, on page 503:&amp;nbsp;26.5 External Crystal / Resonator Connections it says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"When using low-frequency, low-power mode, the only external component is the crystal or ceramic resonator itself. In the other oscillator modes, load capacitors (Cx , Cy ) and feedback resistor (RF) are required."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I conclude from this that Cx, CY and RF are always *required*, with LF-LP being the *only* exception...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the table on the same page suggests that for HF-LP, the "crystal only" configuration can also be used....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone please clarify this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 09:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612306#M36266</guid>
      <dc:creator>johnsmith3</dc:creator>
      <dc:date>2016-11-22T09:33:47Z</dc:date>
    </item>
    <item>
      <title>Re: Contradiction in reference manual K02P64M100SFARM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612307#M36267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When customer using the system oscillator in low-power mode, Rf is integrated and must not be attached externally. So there doesn't need the external feedback resistor.&lt;/P&gt;&lt;P&gt;Customer can select to use the internal load capacitors (Connection 1) or external load capacitors (Connection 3). There doesn't with any restriction when using system oscillator in low-power mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 09:29:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612307#M36267</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-11-25T09:29:09Z</dc:date>
    </item>
    <item>
      <title>Re: Contradiction in reference manual K02P64M100SFARM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612308#M36268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So i can use a 25MHz crystal without external capacitors and without external resistor?&lt;/P&gt;&lt;P&gt;Is this a reliable solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Nov 2016 09:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612308#M36268</guid>
      <dc:creator>johnsmith3</dc:creator>
      <dc:date>2016-11-25T09:36:51Z</dc:date>
    </item>
    <item>
      <title>Re: Contradiction in reference manual K02P64M100SFARM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612309#M36269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, that's right.&lt;/P&gt;&lt;P&gt;Customer can use connection 1 way with a 25MHz crystal, without load capacitors and external feedback resistors.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 03:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Contradiction-in-reference-manual-K02P64M100SFARM/m-p/612309#M36269</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-11-28T03:11:27Z</dc:date>
    </item>
  </channel>
</rss>