<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CRCGEN for K70 Processor in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612291#M36263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alice, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using CRCGEN you can only have one type of output.. So either you use the -o or the -srec.. you can't use both.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So of you use the -srec.. you can then get an s19 record output from crcgen. &amp;nbsp; If you don't have the S19 output from your compiler, there is a&lt;/P&gt;&lt;P&gt;checkbox in the linker Output settings that allows you to create an s19 record.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 26 Feb 2017 04:03:52 GMT</pubDate>
    <dc:creator>Ali2006</dc:creator>
    <dc:date>2017-02-26T04:03:52Z</dc:date>
    <item>
      <title>CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612287#M36259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CRCGEN is not processing my complete compiled file. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My CALC_CRC.CRC file is as follows.&lt;/P&gt;&lt;P&gt;CRC&lt;BR /&gt;SEED = 0xfef&lt;BR /&gt;FILL = 0xFF&lt;BR /&gt;FROM 0x00000000 TO 0x000FFFE0;&lt;BR /&gt;DEST = 0x000FFFE2&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the crcgen running in the post build structure as instructed.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached is the generated S19 from the linker.. as well as the CRC generated file. If you look at address 0x0002EAA0&amp;nbsp; In the .crc file the code ends here an then continues to place the CRC at it's destination and then go on to put out some SRAM default data.&amp;nbsp; In the basic .S19 file the code continues (albiet with a few empty locations to 0x2EAD8 and on to 0x31E68)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried with the linker creating a .afx as well with the same resulting missed location.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337629"&gt;AIMS_ISB_TWR.elf.S19.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337629"&gt;AIMS_ISB_TWR.elf.crc.S19.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 04:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612287#M36259</guid>
      <dc:creator>Ali2006</dc:creator>
      <dc:date>2017-02-08T04:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612288#M36260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;- Could you please tell me How do you generate the SRecord type file &amp;nbsp; .crc.s19 ?&lt;/P&gt;&lt;P&gt;I only can generate crc.elf file.&lt;/P&gt;&lt;P&gt;- Could you please test a simple project to check whether it can work well .&lt;/P&gt;&lt;P&gt;- And there is another method for CRC calculation as Erich said:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/589893"&gt;https://community.nxp.com/message/589893&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 09:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612288#M36260</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-09T09:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612289#M36261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Objectcopy normally generates hex files, there are command line options to generate S19:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OBJCOPY = arm-none-eabi-objcopy&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt; &lt;/SPAN&gt;$(OBJCOPY) --srec-forceS3 -O srec $(OBJDIR)/$&amp;lt; $(OBJDIR)/$@&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRecord may be useful for some CRC's and file conversions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://srecord.sourceforge.net/" title="http://srecord.sourceforge.net/"&gt;SRecord 1.64&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Feb 2017 13:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612289#M36261</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2017-02-09T13:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612290#M36262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- How about your problem now ?&lt;/P&gt;&lt;P&gt;If&amp;nbsp; can now work , I still recommend you use this method :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/" title="https://mcuoneclipse.com/2015/04/26/crc-checksum-generation-with-srecord-tools-for-gnu-and-eclipse/"&gt;CRC Checksum Generation with ‘SRecord’ Tools for GNU and Eclipse | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- And on my side if you use CRCGEN,&amp;nbsp; I still can not use the S19 file to CRC, could you please&lt;/P&gt;&lt;P&gt;send me a simple project , which you have use CRCGEN , I will check and reproduce it on my side, if it have sosme bug, I will report it to the CW team ,thank!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Feb 2017 10:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612290#M36262</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-23T10:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612291#M36263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alice, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using CRCGEN you can only have one type of output.. So either you use the -o or the -srec.. you can't use both.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So of you use the -srec.. you can then get an s19 record output from crcgen. &amp;nbsp; If you don't have the S19 output from your compiler, there is a&lt;/P&gt;&lt;P&gt;checkbox in the linker Output settings that allows you to create an s19 record.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Feb 2017 04:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612291#M36263</guid>
      <dc:creator>Ali2006</dc:creator>
      <dc:date>2017-02-26T04:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612292#M36264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Heather, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your sharing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 07:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612292#M36264</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-27T07:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: CRCGEN for K70 Processor</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612293#M36265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello BOB,&lt;/P&gt;&lt;P&gt;I test a simple project on my side , when use the .elf file , after download the .elf&amp;nbsp; file with CRC ,&lt;/P&gt;&lt;P&gt;except the CRC data , others all the same with .elf without CRC data . So there is no error.&lt;/P&gt;&lt;P&gt;And when I change the .elf with CRC data to SREC file , from the format after the CRC data ,&lt;/P&gt;&lt;P&gt;there seems to some data placed into RAM memory , while this is just format . I think there is&lt;/P&gt;&lt;P&gt;no function error . You can create a simple project to check ,for example a LED, or hello world ,&lt;/P&gt;&lt;P&gt;check whether it can work well .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 08:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRCGEN-for-K70-Processor/m-p/612293#M36265</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-27T08:04:20Z</dc:date>
    </item>
  </channel>
</rss>