<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OPENSDAv2 for KEA128 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610854#M36086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DO you mean the DAP source code is the oepnsdav2 MBED source code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; That code is for the K20 chip, and used as the debugger, just like the FRDM on board debugger with MK20DX128VFM5, when you use the opensda v2.0, and change the firmware to JLINK, then the Jlink firmware will support the KEA128 chip.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 06:30:33 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-09-13T06:30:33Z</dc:date>
    <item>
      <title>OPENSDAv2 for KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610853#M36085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I check the DAP source code, which doesn't include example for TRK-KEA128, pls help check where I could find the resource? thx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 01:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610853#M36085</guid>
      <dc:creator>daweiyou</dc:creator>
      <dc:date>2016-09-13T01:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: OPENSDAv2 for KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610854#M36086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DO you mean the DAP source code is the oepnsdav2 MBED source code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; That code is for the K20 chip, and used as the debugger, just like the FRDM on board debugger with MK20DX128VFM5, when you use the opensda v2.0, and change the firmware to JLINK, then the Jlink firmware will support the KEA128 chip.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 06:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610854#M36086</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-09-13T06:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: OPENSDAv2 for KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610855#M36087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got, thx Kerry.&lt;/P&gt;&lt;P&gt;Yes, I found source code for DAP, but it don't support KEA till now.&lt;/P&gt;&lt;P&gt;&amp;nbsp;The original debugger on TRK-KEA128 is from PE micro.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement simple flasher using DAP source code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Sep 2016 00:33:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OPENSDAv2-for-KEA128/m-p/610855#M36087</guid>
      <dc:creator>daweiyou</dc:creator>
      <dc:date>2016-09-15T00:33:51Z</dc:date>
    </item>
  </channel>
</rss>