<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kl25z spi 9 bits to transmit in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl25z-spi-9-bits-to-transmit/m-p/609850#M36021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the FRDM-KL25Z and want to communicate with &lt;A href="http://www.analog.com/media/en/technical-documentation/data-sheets/HMC6300.pdf"&gt;HMC6300&lt;/A&gt; transmitter.&lt;/P&gt;&lt;P&gt;Here is the time diagram I should produce to have a communication with the component:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6371iFB0A3AD6AE43E37C/image-size/large?v=v2&amp;amp;px=999" title="spi_diagram.png" alt="spi_diagram.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see, I need to send 18 bits using MOSI pin to communicate with the component. 18 is not a multiple of 8 so I don't know what to do with the component to send twice 9 bits or thrice 6 bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to produce such time diagram with the KL25Z?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Oct 2016 16:38:58 GMT</pubDate>
    <dc:creator>raphaelperun</dc:creator>
    <dc:date>2016-10-27T16:38:58Z</dc:date>
    <item>
      <title>kl25z spi 9 bits to transmit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl25z-spi-9-bits-to-transmit/m-p/609850#M36021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the FRDM-KL25Z and want to communicate with &lt;A href="http://www.analog.com/media/en/technical-documentation/data-sheets/HMC6300.pdf"&gt;HMC6300&lt;/A&gt; transmitter.&lt;/P&gt;&lt;P&gt;Here is the time diagram I should produce to have a communication with the component:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6371iFB0A3AD6AE43E37C/image-size/large?v=v2&amp;amp;px=999" title="spi_diagram.png" alt="spi_diagram.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see, I need to send 18 bits using MOSI pin to communicate with the component. 18 is not a multiple of 8 so I don't know what to do with the component to send twice 9 bits or thrice 6 bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to produce such time diagram with the KL25Z?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Oct 2016 16:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl25z-spi-9-bits-to-transmit/m-p/609850#M36021</guid>
      <dc:creator>raphaelperun</dc:creator>
      <dc:date>2016-10-27T16:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: kl25z spi 9 bits to transmit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl25z-spi-9-bits-to-transmit/m-p/609851#M36022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI raphael perun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The diagram you post is not the standard SPI wave, and unfortunately, the KL25 just support 8 bit frame.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, if you want to communicate with this type serial wave, you may need to use the IO to simulate it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have problem, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2016 09:44:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kl25z-spi-9-bits-to-transmit/m-p/609851#M36022</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-10-28T09:44:59Z</dc:date>
    </item>
  </channel>
</rss>