<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 FRDM K64f failing launch sequence</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609699#M36014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two FRDM K64f boards, and I am trying to get CAN communication to work between them, and now one of my boards when I try to program it says that there is a failure in launch sequence. In order to program both boards, I was unplugging one of the boards, so I could program the other, which I think may have to led to this, but I'm not sure how to fix this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if you know how I could program both boards without unplugging one of them that would be helpful as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2017 18:33:26 GMT</pubDate>
    <dc:creator>smith1</dc:creator>
    <dc:date>2017-01-11T18:33:26Z</dc:date>
    <item>
      <title>FRDM K64f failing launch sequence</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609699#M36014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have two FRDM K64f boards, and I am trying to get CAN communication to work between them, and now one of my boards when I try to program it says that there is a failure in launch sequence. In order to program both boards, I was unplugging one of the boards, so I could program the other, which I think may have to led to this, but I'm not sure how to fix this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if you know how I could program both boards without unplugging one of them that would be helpful as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 18:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609699#M36014</guid>
      <dc:creator>smith1</dc:creator>
      <dc:date>2017-01-11T18:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64f failing launch sequence</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609700#M36015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've fixed my issue by resetting the firmware on the board, but are there any suggestions on programming one of boards without unplugging the other?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 00:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609700#M36015</guid>
      <dc:creator>smith1</dc:creator>
      <dc:date>2017-01-12T00:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64f failing launch sequence</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609701#M36016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Timothy Smith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can try the Segger JLINK's method: multiple devices in the scan chain.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; More details, please refer to this document:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.segger.com/admin/uploads/productDocs/UM08001_JLink.pdf" title="https://www.segger.com/admin/uploads/productDocs/UM08001_JLink.pdf"&gt;https://www.segger.com/admin/uploads/productDocs/UM08001_JLink.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Page 180, chapter 5.3 JTAG interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 05:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609701#M36016</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-01-12T05:31:20Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64f failing launch sequence</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609702#M36017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Timothy,&lt;/P&gt;&lt;P&gt;you have to specify different port numbers for each connection, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/" title="https://mcuoneclipse.com/2016/01/23/debug-multiple-boards-with-gdb-at-the-same-time/"&gt;Debug Multiple Boards with GDB at the Same Time | MCU on Eclipse&lt;/A&gt; . Then you can debug multiple boards the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 07:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64f-failing-launch-sequence/m-p/609702#M36017</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-01-12T07:03:10Z</dc:date>
    </item>
  </channel>
</rss>