<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KW31Z constantly resetting in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607857#M35874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here's an update, I'm pretty sure that the problems that I've been seeing is due to bad soldering of the uC to the board.&lt;/P&gt;&lt;P&gt;That big ground plane underneath the part makes it tricky to hand solder these parts onto a board.&lt;/P&gt;&lt;P&gt;The assembler used a hot plate and low temp solder but I'm pretty sure that it did not work as all 3 boards behave differently.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2017 19:43:57 GMT</pubDate>
    <dc:creator>microfirm</dc:creator>
    <dc:date>2017-02-08T19:43:57Z</dc:date>
    <item>
      <title>KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607852#M35869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm bringing up a new virgin MKX31Z board. I have it configured the DCDC converter for auto buck mode.&lt;/P&gt;&lt;P&gt;I'm supplying the VDCDC_IN with 3.6V for an external supply.&lt;/P&gt;&lt;P&gt;The VDD_1P8OUT pin is sitting at 1.7V&lt;/P&gt;&lt;P&gt;The VDD_1P5OUT pin is sitting at 1.64V&lt;/P&gt;&lt;P&gt;The RESET_b line is constantly asserting a 100uS period. It goes high approx 2.5uS and stays lows for approx 97.5uS&lt;/P&gt;&lt;P&gt;I was trying to connect to it w/ a modified FRDM-KW41Z eval board with using the OpenSDA Interface when I found that the new board just sits there constantly driving the RESET_b signal.&lt;/P&gt;&lt;P&gt;There is no way to gain control over the uC with it constantly resetting.&lt;/P&gt;&lt;P&gt;I read through all I can to try and figure out why the reset line would be behaving that way and I can not find anything to help.&lt;/P&gt;&lt;P&gt;What can be going on?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 01:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607852#M35869</guid>
      <dc:creator>microfirm</dc:creator>
      <dc:date>2017-02-07T01:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607853#M35870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is normal behavior for a Kinetis that hasn't been programmed - it shouldn't stop you connecting to it and loading code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 03:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607853#M35870</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-02-07T03:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607854#M35871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone had any luck converting a Freedom Development FRDM-KW41Z into a debugging system able to connect to a virgin uC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 17:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607854#M35871</guid>
      <dc:creator>microfirm</dc:creator>
      <dc:date>2017-02-07T17:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607855#M35872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;do you mean like in &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/" title="https://mcuoneclipse.com/2013/04/27/debug-external-processors-with-usbdm-and-freedom-board/"&gt;Debug External Processors with USBDM and Freedom Board | MCU on Eclipse&lt;/A&gt;&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think this is easily possible, because (on purpose?) the J12 jumper is isolating the OpenSDA from J9 on the FRDM-KW41Z:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14048iD29DD170B46ABCDC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is *different* from other boards where the jmper is isolating the target CPU from the header (e.g. FRDM-KL25Z):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14089i0909FB8AB6A8C7B1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So on the FRDM-KW41Z board you would have to cut the line to the PTA1_SWD_CLK which is not that simple.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 20:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607855#M35872</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-02-07T20:37:14Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607856#M35873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I had to cut a few jumper shorts and wire directly to the K20 signals.&lt;/P&gt;&lt;P&gt;I also tried using a JLINK debugging probe and still can not connect.&lt;/P&gt;&lt;P&gt;I've tried 3 different new boards and to my surprise they all power up with different&lt;/P&gt;&lt;P&gt;VDD_1P8OUT and VDD_1P5OUT levels.&lt;/P&gt;&lt;P&gt;The 1st board I listed above.&lt;/P&gt;&lt;P&gt;The 2nd had the 1P8 out sitting at 500mV and the 3rd is sitting at 2.3V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shouldn't I expect that the default values of 1.8V and 1.5V be the virgin part outputs for the DCDC converter set up for Auto-Buck mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Feb 2017 22:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607856#M35873</guid>
      <dc:creator>microfirm</dc:creator>
      <dc:date>2017-02-07T22:37:28Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607857#M35874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here's an update, I'm pretty sure that the problems that I've been seeing is due to bad soldering of the uC to the board.&lt;/P&gt;&lt;P&gt;That big ground plane underneath the part makes it tricky to hand solder these parts onto a board.&lt;/P&gt;&lt;P&gt;The assembler used a hot plate and low temp solder but I'm pretty sure that it did not work as all 3 boards behave differently.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2017 19:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607857#M35874</guid>
      <dc:creator>microfirm</dc:creator>
      <dc:date>2017-02-08T19:43:57Z</dc:date>
    </item>
    <item>
      <title>Re: KW31Z constantly resetting</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607858#M35875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A little late, but a&amp;nbsp;detailed hardware workaround can be found at&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-333763"&gt;FRDM-KW41Z Development Platform Errata&lt;/A&gt;&amp;nbsp;in the&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;section &lt;STRONG&gt;4) Incorrect routing of SWD clock for stand-alone debugger configuration&lt;/STRONG&gt;.&amp;nbsp;:smileyhappy:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 21:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KW31Z-constantly-resetting/m-p/607858#M35875</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-01-11T21:42:17Z</dc:date>
    </item>
  </channel>
</rss>