<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-64f Interrupt in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-64f-Interrupt/m-p/605653#M35709</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AJAY K R,&lt;/P&gt;&lt;P&gt;You can build and download the SDK_2.1_FRDM-K64F from &lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;MCUXpresso Config Tools&lt;/A&gt;.&lt;BR /&gt;If you want to use UART3, please refer below image then change the codes.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10521i21B781BCC30840AE/image-size/large?v=v2&amp;amp;px=999" title="driver_examples uart.png" alt="driver_examples uart.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Nov 2016 07:02:14 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2016-11-22T07:02:14Z</dc:date>
    <item>
      <title>FRDM-64f Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-64f-Interrupt/m-p/605652#M35708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using FRDM-64F board for my project.I need to get the UART receiving&lt;/P&gt;&lt;P&gt;data whenever it arrives on receive pin.I used UART3 PTC16 and PTC17 pins&lt;/P&gt;&lt;P&gt;for UART and KDS as IDE. I tried several interrupt configuration,which are&lt;/P&gt;&lt;P&gt;not working .Using UART_DRV_ReceiveData for reception which is also&lt;/P&gt;&lt;P&gt;interrupt controlled that also not working.Please help me for solving that&lt;/P&gt;&lt;P&gt;issue.Suggest any other pins, which is available on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-- &lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;AJAY K R&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2016 07:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-64f-Interrupt/m-p/605652#M35708</guid>
      <dc:creator>ajaykr</dc:creator>
      <dc:date>2016-11-21T07:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-64f Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-64f-Interrupt/m-p/605653#M35709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AJAY K R,&lt;/P&gt;&lt;P&gt;You can build and download the SDK_2.1_FRDM-K64F from &lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;MCUXpresso Config Tools&lt;/A&gt;.&lt;BR /&gt;If you want to use UART3, please refer below image then change the codes.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10521i21B781BCC30840AE/image-size/large?v=v2&amp;amp;px=999" title="driver_examples uart.png" alt="driver_examples uart.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 07:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-64f-Interrupt/m-p/605653#M35709</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-11-22T07:02:14Z</dc:date>
    </item>
  </channel>
</rss>