<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Generate Tone frequency using GPIO Pin in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604553#M35588</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mayur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll repeat a final time that DMA is the way to do it as shown a number of times now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you are not making any progress after what looks like 3 weeks from your original question, why not simply change the pin used on the HW to one that allows the FTM to be used? This HW modification probably costs less that the SW development/workaround in the long run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also remember when the next HW is designed to connect pins suitably to make use of the processor's HW capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 11:09:52 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2016-12-14T11:09:52Z</dc:date>
    <item>
      <title>Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604544#M35579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using MK22Fx512 controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was trying to generate Frequency using PIT timer. its working some frequency but not all. We need to generate frequency between 2k to 4k Hz. I am getting some noise intermediate.&lt;/P&gt;&lt;P&gt;Please suggest me how to resolve this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Mayur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 09:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604544#M35579</guid>
      <dc:creator>mayursavaj</dc:creator>
      <dc:date>2016-12-13T09:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604545#M35580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mayur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned in your other thread, the only serious way to use&amp;nbsp; a PIT channel to generate a stable frequency on a GPIO pin is to use DMA: &lt;A href="https://community.nxp.com/thread/439603"&gt;Generate Frequency using GPIO Pin&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you prefer to use interrupts, for example, you may need to accept some jitter/noise; If your only possibility is to use interrupts make sure that you give the interrupt highest priority and, where possible, don't globally block the interrupt when other interrupts are handled or in critical code regions (use the interrupt mask setting rather than global interrupt mask).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Generally I still maintain that resorting to interrupts when DMA is a fairly simple possibility (I already posted code for it which operates on all GPIOs on all Kinetis parts with a free DMA channel) is poor practice, only for use in hobby projects and not in professional product design.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 12:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604545#M35580</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-12-13T12:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604546#M35581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A PIT timer appears to be more optimized for internal peripheral timing, it doesn't appear to have a hardware connection to a I/O pin so you have to toggle a GPIO. Can you use a general purpose timer and PWM output instead? That way interrupt latency and other interrupt events in your processor wont get in the way of the pin toggling on time. What you are seeing now are other events blocking and delaying the pin from toggling.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 12:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604546#M35581</guid>
      <dc:creator>markwyman</dc:creator>
      <dc:date>2016-12-13T12:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604547#M35582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mayur,&lt;/P&gt;&lt;P&gt;The PPG_LDD can be used generated PWM signal from 2kHz to 4kHz. It was based on modify the FTMx_MOD of FTM module. If you don't want to use the code generated by Processor Expert, you can also use the FTM examples in &lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/freedom-development-boards/software-development-kit-for-kinetis-mcus:KINETIS-SDK"&gt;Kinetis SDK V2&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10679i22A83CE2F4E894CA/image-size/large?v=v2&amp;amp;px=999" title="PPG_LDD PPG1_SetFrequencyHz.png" alt="PPG_LDD PPG1_SetFrequencyHz.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If you are using MK22FX512VLL12, it have four FTM modules. So I am not sure why you want to generate Tone frequency using GPIO instead of using FTM module.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10772i0EBDD7731CF31636/image-size/large?v=v2&amp;amp;px=999" title="MK22FX512VLL12 FTM0-FTM3.png" alt="MK22FX512VLL12 FTM0-FTM3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And MK22FX512VLL12 is Not Recommended for New Design, please &lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/k-series-performance-m4/k2x-usb/kinetis-k22-120-mhz-cost-effective-full-speed-usb-microcontrollers-mcus-based-on-arm-cortex-m4-core:K22_120?&amp;amp;cof=0&amp;amp;am=0&amp;amp;mvf=p779~LQFP&amp;amp;rf=p119~100_H,p119~100_L&amp;amp;tab=Buy_Parametric_Tab"&gt;select another K22&lt;/A&gt; MCU.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10936i36E5D851BED40CD5/image-size/large?v=v2&amp;amp;px=999" title="Not Recommended for New Design.png" alt="Not Recommended for New Design.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 06:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604547#M35582</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-12-14T06:35:04Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604548#M35583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using MK22Fx512VLL12. But my issue is that buzzer don't have FTM functionality.So I have use as a GPIO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11134i9A58CB6085937018/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 07:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604548#M35583</guid>
      <dc:creator>mayursavaj</dc:creator>
      <dc:date>2016-12-14T07:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604549#M35584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;Can I use GPIO pin as PWM (if Pin don't have that capability)? If yes than please send me some example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mayur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 07:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604549#M35584</guid>
      <dc:creator>mayursavaj</dc:creator>
      <dc:date>2016-12-14T07:08:53Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604550#M35585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mayur,&lt;/P&gt;&lt;P&gt;I don't know the type of your buzzer.&lt;/P&gt;&lt;P&gt;Do you want a waveform to drive the buzzer like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11299i5636EA235F95C7D0/image-size/large?v=v2&amp;amp;px=999" title="piezo-buzzer-circuit.png" alt="piezo-buzzer-circuit.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The FTM module can be used output waveform with 3.3v. And the PPG1_SetFrequencyHz can be used to change the frequency of waveform at runtime.&lt;/P&gt;&lt;P&gt;The PPG_LDD can be used to output PWM waveform with 50% Ratio. You can set the Ratio to 50% using PPG1_SetRatio16 function. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11444i154DD92CE956F913/image-size/large?v=v2&amp;amp;px=999" title="Example of generated signal PPG_LDD.png" alt="Example of generated signal PPG_LDD.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pin with FTMx_CHx have that capability. For example Pin93 PTD2.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11497i27E8DC5289C79EB3/image-size/large?v=v2&amp;amp;px=999" title="FTM3_CH0 pin93.png" alt="FTM3_CH0 pin93.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And would you please tell us which pin are you using? Or can you select another pin with FTM capability?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;---------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 08:19:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604550#M35585</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-12-14T08:19:12Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604551#M35586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Pin 90. We can't change Pin because all other pins have connected to other peripheral.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 09:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604551#M35586</guid>
      <dc:creator>mayursavaj</dc:creator>
      <dc:date>2016-12-14T09:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604552#M35587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to data sheet pin 90 don't have FTM capability.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me alternate method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mayur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 09:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604552#M35587</guid>
      <dc:creator>mayursavaj</dc:creator>
      <dc:date>2016-12-14T09:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: Generate Tone frequency using GPIO Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604553#M35588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mayur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll repeat a final time that DMA is the way to do it as shown a number of times now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you are not making any progress after what looks like 3 weeks from your original question, why not simply change the pin used on the HW to one that allows the FTM to be used? This HW modification probably costs less that the SW development/workaround in the long run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also remember when the next HW is designed to connect pins suitably to make use of the processor's HW capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 11:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Generate-Tone-frequency-using-GPIO-Pin/m-p/604553#M35588</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-12-14T11:09:52Z</dc:date>
    </item>
  </channel>
</rss>