<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 KM33Z128 boots in VLPR mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM33Z128-boots-in-VLPR-mode/m-p/604371#M35569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working in a project that uses the microcontroller KM33Z128AM. I realized that some chips are booting randomly in VLPR mode. After that, when configuring the clock, the devices performs a reset. The device then enters in a infinite loop of resets. The bit EXE_MODE in FTFL_OPT register is zero. Therefore, I think the microcontroller should be always exit from reset in RUN mode. In which other situation could the device boot in VLPR mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2016 08:12:04 GMT</pubDate>
    <dc:creator>miguelportela</dc:creator>
    <dc:date>2016-12-13T08:12:04Z</dc:date>
    <item>
      <title>KM33Z128 boots in VLPR mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM33Z128-boots-in-VLPR-mode/m-p/604371#M35569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am working in a project that uses the microcontroller KM33Z128AM. I realized that some chips are booting randomly in VLPR mode. After that, when configuring the clock, the devices performs a reset. The device then enters in a infinite loop of resets. The bit EXE_MODE in FTFL_OPT register is zero. Therefore, I think the microcontroller should be always exit from reset in RUN mode. In which other situation could the device boot in VLPR mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 08:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM33Z128-boots-in-VLPR-mode/m-p/604371#M35569</guid>
      <dc:creator>miguelportela</dc:creator>
      <dc:date>2016-12-13T08:12:04Z</dc:date>
    </item>
  </channel>
</rss>