<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB Audio speaker in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Audio-speaker/m-p/603460#M35488</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I used FRDM-K66F to created a USB audio speaker application based on K21F KSDK 2.0 USB example code.&lt;/P&gt;&lt;P&gt;Basically the function is works in 16bit/16kHz, but when I try to increase the sample rate to 48kHz.&lt;/P&gt;&lt;P&gt;The function is not works.&lt;/P&gt;&lt;P&gt;Is there any one have similar experience before?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Mar 2017 08:42:21 GMT</pubDate>
    <dc:creator>kyleyang</dc:creator>
    <dc:date>2017-03-21T08:42:21Z</dc:date>
    <item>
      <title>USB Audio speaker</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Audio-speaker/m-p/603460#M35488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I used FRDM-K66F to created a USB audio speaker application based on K21F KSDK 2.0 USB example code.&lt;/P&gt;&lt;P&gt;Basically the function is works in 16bit/16kHz, but when I try to increase the sample rate to 48kHz.&lt;/P&gt;&lt;P&gt;The function is not works.&lt;/P&gt;&lt;P&gt;Is there any one have similar experience before?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Mar 2017 08:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Audio-speaker/m-p/603460#M35488</guid>
      <dc:creator>kyleyang</dc:creator>
      <dc:date>2017-03-21T08:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: USB Audio speaker</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Audio-speaker/m-p/603461#M35489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer also could refer KSDK software for TWR-K65F180M board [usb dev_audio_speaker] demo.&lt;/P&gt;&lt;P&gt;For the FRDM-K66F use the different codec chip DA7212, customer need to check the DA7212 codec driver related codes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 05:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Audio-speaker/m-p/603461#M35489</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-03-24T05:27:04Z</dc:date>
    </item>
  </channel>
</rss>