<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Use J-link programmer to program MKL04Z16VFM4, failed to connect</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-J-link-programmer-to-program-MKL04Z16VFM4-failed-to-connect/m-p/603427#M35487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fish,&lt;/P&gt;&lt;P&gt;Hold down the Reset Button then try to connect the MCU using JLink Commander. Release the Reset Button if you can establish a connection to target.&lt;BR /&gt;The KL04 only support SWD, please don't select JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the hardware:&lt;/P&gt;&lt;P&gt;The RESET_b pin should have a 100 nF capacitor close to the MCU for transient protection. An external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;BR /&gt;The NMI_b pin must not have any capacitance connected to it. An external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;SWD_DIO: an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;BR /&gt;SWD_CLK: float or an external 4.7 kΩ to 10 kΩ pulldown is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2017 13:00:29 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-01-11T13:00:29Z</dc:date>
    <item>
      <title>Use J-link programmer to program MKL04Z16VFM4, failed to connect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-J-link-programmer-to-program-MKL04Z16VFM4-failed-to-connect/m-p/603426#M35486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use J-link programmer to program MKL04Z16VFM4, failed to connect, could not establish a connection to target. We can sure the wiring connection is right, could you please help to confirm why happen this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 08:28:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-J-link-programmer-to-program-MKL04Z16VFM4-failed-to-connect/m-p/603426#M35486</guid>
      <dc:creator>fishwang</dc:creator>
      <dc:date>2017-01-10T08:28:20Z</dc:date>
    </item>
    <item>
      <title>Re: Use J-link programmer to program MKL04Z16VFM4, failed to connect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-J-link-programmer-to-program-MKL04Z16VFM4-failed-to-connect/m-p/603427#M35487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fish,&lt;/P&gt;&lt;P&gt;Hold down the Reset Button then try to connect the MCU using JLink Commander. Release the Reset Button if you can establish a connection to target.&lt;BR /&gt;The KL04 only support SWD, please don't select JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the hardware:&lt;/P&gt;&lt;P&gt;The RESET_b pin should have a 100 nF capacitor close to the MCU for transient protection. An external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;BR /&gt;The NMI_b pin must not have any capacitance connected to it. An external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;SWD_DIO: an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;BR /&gt;SWD_CLK: float or an external 4.7 kΩ to 10 kΩ pulldown is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 13:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-J-link-programmer-to-program-MKL04Z16VFM4-failed-to-connect/m-p/603427#M35487</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-01-11T13:00:29Z</dc:date>
    </item>
  </channel>
</rss>