<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC callback for KE02 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602862#M35440</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Sorry for the late reply!&lt;/P&gt;&lt;P&gt;This MCU doesn't have such a Register which include Channel Conversion Complete Flag.&lt;/P&gt;&lt;P&gt;Have you try to use the ADC_FIFO_demo in KEXX_DRIVERS_V1.2.1_DEVD.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14919i608ED837B06818B4/image-size/large?v=v2&amp;amp;px=999" title="ADC_FIFO_demo.png" alt="ADC_FIFO_demo.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Feb 2017 03:09:53 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-02-14T03:09:53Z</dc:date>
    <item>
      <title>ADC callback for KE02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602861#M35439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read values from the multiple ADC channels in interrupt mode. From the kexx_drv_lib, ADC_SetCallBack() sets the callback function and ADC_SetChannel() sets ADC channel. Can I set the multiple channels and then know which channel the value with&amp;nbsp;ADC_ReadResultReg() is from in callback function?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Code example:&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_SetCallBack(ADC_CallBack);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_Init(ADC, &amp;amp;sADC_Config);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_SetChannel(ADC,ADC_CHANNEL_AD2)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_SetChannel(ADC,ADC_CHANNEL_AD3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_SetChannel(ADC,ADC_CHANNEL_AD4)&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;void ADC_CallBack( void )&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Which ADC channel is this result from? Any function can be used?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint16_t result = ADC_ReadResultReg(ADC);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 11:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602861#M35439</guid>
      <dc:creator>adam_zhou</dc:creator>
      <dc:date>2017-02-04T11:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: ADC callback for KE02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602862#M35440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Sorry for the late reply!&lt;/P&gt;&lt;P&gt;This MCU doesn't have such a Register which include Channel Conversion Complete Flag.&lt;/P&gt;&lt;P&gt;Have you try to use the ADC_FIFO_demo in KEXX_DRIVERS_V1.2.1_DEVD.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14919i608ED837B06818B4/image-size/large?v=v2&amp;amp;px=999" title="ADC_FIFO_demo.png" alt="ADC_FIFO_demo.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 03:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602862#M35440</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-02-14T03:09:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADC callback for KE02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602863#M35441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Robin, you're right. ADC_FIFO_demo can work for me. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2017 14:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-callback-for-KE02/m-p/602863#M35441</guid>
      <dc:creator>adam_zhou</dc:creator>
      <dc:date>2017-02-14T14:26:53Z</dc:date>
    </item>
  </channel>
</rss>