<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: frdm-kl25z emulator connection fails when using swd</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kl25z-emulator-connection-fails-when-using-swd/m-p/602830#M35434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;why did you cut J11? This is only needed if you want to use the FRDM board to debug *another* board, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;Using the Freedom Board as SWD Programmer | MCU on Eclipse&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;To debug the KL25Z on the FRDM-KL25Z using the SWD connector, all what you ahve to do is to add that connector, nothing else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Feb 2017 15:49:35 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2017-02-27T15:49:35Z</dc:date>
    <item>
      <title>frdm-kl25z emulator connection fails when using swd</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kl25z-emulator-connection-fails-when-using-swd/m-p/602829#M35433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm unable to get emulator to connect to the frdm-kl25z. I'm using j-link emulator. I have cut the trace on J11 as instructed. The debugging via openSDA works ok. When I try to connect with Segger J-Flash (target-&amp;gt;connect) it says "failed to connect". Similar thing happend when I try start debugging in&amp;nbsp; IAR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 14:17:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kl25z-emulator-connection-fails-when-using-swd/m-p/602829#M35433</guid>
      <dc:creator>tuomasaaltio</dc:creator>
      <dc:date>2017-02-27T14:17:10Z</dc:date>
    </item>
    <item>
      <title>Re: frdm-kl25z emulator connection fails when using swd</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kl25z-emulator-connection-fails-when-using-swd/m-p/602830#M35434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;why did you cut J11? This is only needed if you want to use the FRDM board to debug *another* board, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="https://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;Using the Freedom Board as SWD Programmer | MCU on Eclipse&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;To debug the KL25Z on the FRDM-KL25Z using the SWD connector, all what you ahve to do is to add that connector, nothing else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Feb 2017 15:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/frdm-kl25z-emulator-connection-fails-when-using-swd/m-p/602830#M35434</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-02-27T15:49:35Z</dc:date>
    </item>
  </channel>
</rss>