<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックUSB Port of K60</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Port-of-K60/m-p/212198#M3528</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm developing a new project based on K60 device and I would like implement two USB interface. One in FS mode, using internal FS PHY and one in HS mode using external PHY. Could they work together or there are some restriction.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that HS mode port could work in HOST configuration with DMA forward internal RAM of K60, just to satisfy a input data rate of 50Mbit/s.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Mar 2012 18:57:58 GMT</pubDate>
    <dc:creator>leofavilli</dc:creator>
    <dc:date>2012-03-02T18:57:58Z</dc:date>
    <item>
      <title>USB Port of K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Port-of-K60/m-p/212198#M3528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I'm developing a new project based on K60 device and I would like implement two USB interface. One in FS mode, using internal FS PHY and one in HS mode using external PHY. Could they work together or there are some restriction.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that HS mode port could work in HOST configuration with DMA forward internal RAM of K60, just to satisfy a input data rate of 50Mbit/s.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2012 18:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-Port-of-K60/m-p/212198#M3528</guid>
      <dc:creator>leofavilli</dc:creator>
      <dc:date>2012-03-02T18:57:58Z</dc:date>
    </item>
  </channel>
</rss>