<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFRDM K64 - buffers on I/O</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-buffers-on-I-O/m-p/599231#M35171</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Regarding the available I/O's on this board, I've noticed there are no buffers on the signal I/O's. I've looked at Arduino R3 (because it can connect to it) but didn't find any buffers over there also. Am I missing something here?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because I think it is not a good practice design to neglect the buffers on I/O signals, in case there's some kind of problem.&lt;/P&gt;&lt;P&gt;It seems the I/O's are connected directly from the K64 to Arduino.&lt;/P&gt;&lt;P&gt;Thx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Dec 2016 21:37:51 GMT</pubDate>
    <dc:creator>roymessinger</dc:creator>
    <dc:date>2016-12-09T21:37:51Z</dc:date>
    <item>
      <title>FRDM K64 - buffers on I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-buffers-on-I-O/m-p/599231#M35171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Regarding the available I/O's on this board, I've noticed there are no buffers on the signal I/O's. I've looked at Arduino R3 (because it can connect to it) but didn't find any buffers over there also. Am I missing something here?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Because I think it is not a good practice design to neglect the buffers on I/O signals, in case there's some kind of problem.&lt;/P&gt;&lt;P&gt;It seems the I/O's are connected directly from the K64 to Arduino.&lt;/P&gt;&lt;P&gt;Thx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 21:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-buffers-on-I-O/m-p/599231#M35171</guid>
      <dc:creator>roymessinger</dc:creator>
      <dc:date>2016-12-09T21:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64 - buffers on I/O</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-buffers-on-I-O/m-p/599232#M35172</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roy,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you mean the buffter on I/O is the GPIO buffer?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The input GPIO buffer is the GPIOx_PDIR, when you receive the data, you can use the code save the GPIO data to elsewhere you want, no matter RAM, FLASH or external flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; The ouput GPIO buffer is the same, when you want to send the data, just set the according data in K64 register GPIOx_PDOR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 06:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-buffers-on-I-O/m-p/599232#M35172</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-12-12T06:29:38Z</dc:date>
    </item>
  </channel>
</rss>