<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Achieving max ADC sampling rate on the K60</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211807#M3513</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you found any information on this? &amp;nbsp;I have found in a couple of different places where it is stated that a couple of the ADC inputs are routed to both internal ADC's (on the K60) and the samples can be interleaved for a higher sample rate. &amp;nbsp;But other than stating that it can be done I have found no documentation reporting how it is done or if there is a way to synchronize the two ADC's with each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Apr 2012 05:08:12 GMT</pubDate>
    <dc:creator>hubje3</dc:creator>
    <dc:date>2012-04-24T05:08:12Z</dc:date>
    <item>
      <title>Achieving max ADC sampling rate on the K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211806#M3512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am trying to achieve the maximum sampling rate of 818.330 ksps for the K60&lt;BR /&gt;&lt;BR /&gt;the "K60P144M100SF2 K60 Sub-Family Data Sheet" state that this is for the following conditions&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;EM&gt;≤ 13 bit modes&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;No ADC hardware averaging&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;Continuous conversions enabled, subsequent conversion time&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;so I have 2 questions&lt;BR /&gt;&lt;BR /&gt;1) Could you point me to a reference explaining clearly what the ADC continuous mode is?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; - trigger once and then it keeps going, generating an interrupt after each measurement is complete ? no hw average&lt;BR /&gt;&amp;nbsp; &amp;nbsp; - how do you stop it?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; - if you start 2 channels at the same time, will the measurements stay "synchronized"?&lt;BR /&gt;&amp;nbsp; &amp;nbsp; - ... &amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;2) Do you have a sample project that shows how to achieve this sampling rate?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bernard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2012 22:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211806#M3512</guid>
      <dc:creator>BernardSeller</dc:creator>
      <dc:date>2012-03-01T22:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: Achieving max ADC sampling rate on the K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211807#M3513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you found any information on this? &amp;nbsp;I have found in a couple of different places where it is stated that a couple of the ADC inputs are routed to both internal ADC's (on the K60) and the samples can be interleaved for a higher sample rate. &amp;nbsp;But other than stating that it can be done I have found no documentation reporting how it is done or if there is a way to synchronize the two ADC's with each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2012 05:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211807#M3513</guid>
      <dc:creator>hubje3</dc:creator>
      <dc:date>2012-04-24T05:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: Achieving max ADC sampling rate on the K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211808#M3514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you using MQX? The MQX A/D driver is worthless. Seems like there's a lot of issues with it and I've seen aboslutely no support for it on the forums.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2012 04:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211808#M3514</guid>
      <dc:creator>dan_quist</dc:creator>
      <dc:date>2012-07-20T04:24:13Z</dc:date>
    </item>
    <item>
      <title>Re: Achieving max ADC sampling rate on the K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211809#M3515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A couple things I have learned about the ADC, first, each channel is capable of the full speed stated in the manual and&amp;nbsp;you do not need to interleave the samples in order to get that speed. &amp;nbsp;In order to actually retrieve the data that fast you will have to use DMA, even an ISR based driver isn't going to be fast enough.&lt;/P&gt;&lt;P&gt;Second, in order to get that full speed you need to have an 18 MHz clock driving the ADC, that means your system has to be running at a multiple of 18 MHz (i.e. 72 MHz). &amp;nbsp;I can't remember if there is an option for an external clock, but that might be an option to run the system at 100MHz and still have the full speed of the ADC.&lt;/P&gt;&lt;P&gt;Using a custom&amp;nbsp;ADC&amp;nbsp;driver with MQX&amp;nbsp;the&amp;nbsp;sample rate of&amp;nbsp;my system is&amp;nbsp;about 700ksps with the limiting factor being the clock driving the ADC (my system is running at 96MHz).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Jeremy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2012 22:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Achieving-max-ADC-sampling-rate-on-the-K60/m-p/211809#M3515</guid>
      <dc:creator>hubje3</dc:creator>
      <dc:date>2012-07-24T22:52:58Z</dc:date>
    </item>
  </channel>
</rss>