<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: ADC INIT MK02</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-INIT-MK02/m-p/597132#M34969</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jack,&lt;/P&gt;&lt;P&gt;I think You can call the following function in this way:&lt;/P&gt;&lt;P&gt;ADC16_SetChannelMuxMode(ADC0,kADC16_ChannelMuxA); or ADC16_SetChannelMuxMode(ADC0,kADC16_ChannelMuxB);&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void ADC16_SetChannelMuxMode(ADC_Type *base, adc16_channel_mux_mode_t mode)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kADC16_ChannelMuxA == mode)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; base-&amp;gt;CFG2 &amp;amp;= ~ADC_CFG2_MUXSEL_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else /* kADC16_ChannelMuxB. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; base-&amp;gt;CFG2 |= ADC_CFG2_MUXSEL_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Sep 2016 02:53:06 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-09-08T02:53:06Z</dc:date>
    <item>
      <title>ADC INIT MK02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-INIT-MK02/m-p/597131#M34968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can init most&amp;nbsp;adc channel like the following&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;ADC16_GetDefaultConfig(&amp;amp;adc16ConfigStruct);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;ADC16_Init(DEMO_ADC16_BASE, &amp;amp;adc16ConfigStruct);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;ADC16_EnableHardwareTrigger(DEMO_ADC16_BASE, false); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;/* Make sure the software trigger is used. */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC16_HAS_CALIBRATION) &amp;amp;&amp;amp; FSL_FEATURE_ADC16_HAS_CALIBRATION&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;if (kStatus_Success == ADC16_DoAutoCalibration(DEMO_ADC16_BASE))&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PRINTF("ADC16_DoAutoCalibration() Done.\r\n");&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;else&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PRINTF("ADC16_DoAutoCalibration() Failed.\r\n");&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt;#endif /* FSL_FEATURE_ADC16_HAS_CALIBRATION */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;adc16ChannelConfigStruct.channelNumber = DEMO_ADC16_USER_CHANNEL;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;adc16ChannelConfigStruct.enableInterruptOnConversionCompleted = false;&lt;BR /&gt;#if defined(FSL_FEATURE_ADC16_HAS_DIFF_MODE) &amp;amp;&amp;amp; FSL_FEATURE_ADC16_HAS_DIFF_MODE&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;adc16ChannelConfigStruct.enableDifferentialConversion = false;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC16_HAS_DIFF_MODE */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but how to init the channel se4a, channel 4b,channel se5a, channel se5b etc&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; how to init the channel DM0, channel DP0 etc (the same using as channel se0)&lt;/P&gt;&lt;P&gt;or how to init&amp;nbsp;the temp sensor?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5378i6AF554DDFF219F80/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5426iB0117DFE3DB41A8B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;-Jack&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 05:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-INIT-MK02/m-p/597131#M34968</guid>
      <dc:creator>jackxu</dc:creator>
      <dc:date>2016-09-07T05:37:22Z</dc:date>
    </item>
    <item>
      <title>Re: ADC INIT MK02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-INIT-MK02/m-p/597132#M34969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jack,&lt;/P&gt;&lt;P&gt;I think You can call the following function in this way:&lt;/P&gt;&lt;P&gt;ADC16_SetChannelMuxMode(ADC0,kADC16_ChannelMuxA); or ADC16_SetChannelMuxMode(ADC0,kADC16_ChannelMuxB);&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void ADC16_SetChannelMuxMode(ADC_Type *base, adc16_channel_mux_mode_t mode)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kADC16_ChannelMuxA == mode)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; base-&amp;gt;CFG2 &amp;amp;= ~ADC_CFG2_MUXSEL_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else /* kADC16_ChannelMuxB. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; base-&amp;gt;CFG2 |= ADC_CFG2_MUXSEL_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 02:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-INIT-MK02/m-p/597132#M34969</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-08T02:53:06Z</dc:date>
    </item>
  </channel>
</rss>