<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Start My Design</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Start-My-Design/m-p/595926#M34910</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently started to work with the Kinetis devices, for my first project I used the K64 FRDM board, that was good to get familiar with the chip, tools, PE and KSDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my second project I downloaded the BXL files and was able to import them into Altium. I created a basic board that I can use for multiple projects using the K26, the board has a USB port added, a couple of switches, LEDs and the debug connector, just a minimum setup. I used the schematics from the demo boards to check what I had included.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Agreed, it could have been easier if the minimum chip setup circuitry had been shown in a data sheet like it used to be, this would be good for an application note.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jul 2016 14:14:57 GMT</pubDate>
    <dc:creator>therealfreegeek</dc:creator>
    <dc:date>2016-07-21T14:14:57Z</dc:date>
    <item>
      <title>Start My Design</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Start-My-Design/m-p/595925#M34909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I want to learn designing projects with &lt;STRONG&gt;arm&lt;/STRONG&gt;. As I don't want to use the &lt;STRONG&gt;dev boards&lt;/STRONG&gt;, I want to obtain my design. Since there is almost &lt;STRONG&gt;zero information&lt;/STRONG&gt; about designing arm boards and companies like NXP provides &lt;STRONG&gt;nothing&lt;/STRONG&gt; about this. I keep asking to &lt;STRONG&gt;forums&lt;/STRONG&gt; etc. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are famous tools engineers use for designing their boards like &lt;STRONG&gt;Proteus, Altium&lt;/STRONG&gt; etc. Is there a documentation about using them to &lt;STRONG&gt;create ARM projects&lt;/STRONG&gt;? I can't even use &lt;STRONG&gt;Kinetis schematics provided by NXP&lt;/STRONG&gt; since they only supply them in &lt;STRONG&gt;.bxl&lt;/STRONG&gt; format. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am totally &lt;STRONG&gt;exhausted&lt;/STRONG&gt; of being supposed to search so hard for any bit of information on this area. I don't understand, do companies &lt;STRONG&gt;not&lt;/STRONG&gt; want new people to learn and develop projects?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 13:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Start-My-Design/m-p/595925#M34909</guid>
      <dc:creator>mertdenizpolat</dc:creator>
      <dc:date>2016-07-21T13:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: Start My Design</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Start-My-Design/m-p/595926#M34910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently started to work with the Kinetis devices, for my first project I used the K64 FRDM board, that was good to get familiar with the chip, tools, PE and KSDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my second project I downloaded the BXL files and was able to import them into Altium. I created a basic board that I can use for multiple projects using the K26, the board has a USB port added, a couple of switches, LEDs and the debug connector, just a minimum setup. I used the schematics from the demo boards to check what I had included.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Agreed, it could have been easier if the minimum chip setup circuitry had been shown in a data sheet like it used to be, this would be good for an application note.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 14:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Start-My-Design/m-p/595926#M34910</guid>
      <dc:creator>therealfreegeek</dc:creator>
      <dc:date>2016-07-21T14:14:57Z</dc:date>
    </item>
  </channel>
</rss>