<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Number of flexio peripherals on kl17?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594573#M34869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FlexIO can only do one thing at a time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 11:53:01 GMT</pubDate>
    <dc:creator>bobpaddock</dc:creator>
    <dc:date>2016-09-06T11:53:01Z</dc:date>
    <item>
      <title>Number of flexio peripherals on kl17?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594572#M34868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Can somebody please confirm the number of flexio peripherals supported by KL17? According to the &lt;A href="http://cache.nxp.com/files/32bit/doc/data_sheet/KL17P64M48SF6.pdf"&gt;document&lt;/A&gt;&amp;nbsp;it supports&lt;/P&gt;&lt;P&gt;" &lt;EM&gt;One FlexIO module supporting emulation of&amp;nbsp;additional UART, IrDA, SPI, I2C, I2S, PWM and&amp;nbsp;other serial modules, etc.&lt;/EM&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean 1 FlexIO module supporting multiple serial modules at same time (eg Uart and I2C simulataneously or &amp;nbsp;2 I2C simulataneously)?&lt;/P&gt;&lt;P&gt;Or&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 FlexIO module supporting 1 of the serial module? (Eg : 1 FlexIO UART or 1 FlexIO I2C)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the reference manual, there is only 1 FLexIO&amp;nbsp;base address "0x4005_F000".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many Thanks,&lt;/P&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 11:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594572#M34868</guid>
      <dc:creator>tonymakkiel</dc:creator>
      <dc:date>2016-09-06T11:50:42Z</dc:date>
    </item>
    <item>
      <title>Re: Number of flexio peripherals on kl17?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594573#M34869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FlexIO can only do one thing at a time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 11:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594573#M34869</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2016-09-06T11:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: Number of flexio peripherals on kl17?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594574#M34870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the quick reply Bob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean flexIO needs to be reconfigured run time if it needs to support another module?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was hoping to have 2 I2C masters using flexio. with 2 different set of pins configured(eg: PORTD6 and PORTD7 for bus 1 and PORTD0 and PORTD1 for bus 2 ). I guess that is not possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 12:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594574#M34870</guid>
      <dc:creator>tonymakkiel</dc:creator>
      <dc:date>2016-09-06T12:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: Number of flexio peripherals on kl17?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594575#M34871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FlexIO gets you one additional peripheral.&lt;BR /&gt;While probably not impossible, I'd say it is impractical to try to use it for two things at once even if they are both I2C.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 12:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594575#M34871</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2016-09-06T12:23:28Z</dc:date>
    </item>
    <item>
      <title>Re: Number of flexio peripherals on kl17?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594576#M34872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Bob Paddock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 14:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Number-of-flexio-peripherals-on-kl17/m-p/594576#M34872</guid>
      <dc:creator>tonymakkiel</dc:creator>
      <dc:date>2016-09-06T14:27:09Z</dc:date>
    </item>
  </channel>
</rss>