<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックPull-up/down resistors for UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pull-up-down-resistors-for-UART/m-p/594059#M34859</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Could you please advise if it's correct to connect MK10 to MKM33 without external pull-up or pull-down resistors?&lt;/P&gt;&lt;P&gt;Please find attached the block diagram.&lt;/P&gt;&lt;P&gt;Here we connect main MCU &lt;SPAN style="font-size: 11.0pt;"&gt;MK10DX256VLK7 &lt;/SPAN&gt;to the metering MCU &lt;SPAN style="font-size: 11.0pt;"&gt;MKM33Z128ACLH5 &lt;/SPAN&gt;and set UART0_TX pin for output, and PTI0 pin for input with internal pull-up/down.&lt;/P&gt;&lt;P&gt;When data goes from &lt;SPAN style="font-size: 11.0pt;"&gt;MKM33Z128ACLH5&amp;nbsp; to MK10DX256VLK7&amp;nbsp; we set PTI0 as output, and UART0_RX as input with internal pull-up/down.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Resistors R50 and R53 are used for nanosecond noise elimination. Vcc is is 3.3V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Could you please advise if this implementation is correct or we need to add external pull-up/down resistors?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Alexey&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 12:11:48 GMT</pubDate>
    <dc:creator>alexeypanteleyc</dc:creator>
    <dc:date>2016-09-06T12:11:48Z</dc:date>
    <item>
      <title>Pull-up/down resistors for UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pull-up-down-resistors-for-UART/m-p/594059#M34859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Could you please advise if it's correct to connect MK10 to MKM33 without external pull-up or pull-down resistors?&lt;/P&gt;&lt;P&gt;Please find attached the block diagram.&lt;/P&gt;&lt;P&gt;Here we connect main MCU &lt;SPAN style="font-size: 11.0pt;"&gt;MK10DX256VLK7 &lt;/SPAN&gt;to the metering MCU &lt;SPAN style="font-size: 11.0pt;"&gt;MKM33Z128ACLH5 &lt;/SPAN&gt;and set UART0_TX pin for output, and PTI0 pin for input with internal pull-up/down.&lt;/P&gt;&lt;P&gt;When data goes from &lt;SPAN style="font-size: 11.0pt;"&gt;MKM33Z128ACLH5&amp;nbsp; to MK10DX256VLK7&amp;nbsp; we set PTI0 as output, and UART0_RX as input with internal pull-up/down.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Resistors R50 and R53 are used for nanosecond noise elimination. Vcc is is 3.3V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Could you please advise if this implementation is correct or we need to add external pull-up/down resistors?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Thanks and regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Alexey&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 12:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pull-up-down-resistors-for-UART/m-p/594059#M34859</guid>
      <dc:creator>alexeypanteleyc</dc:creator>
      <dc:date>2016-09-06T12:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: Pull-up/down resistors for UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pull-up-down-resistors-for-UART/m-p/594060#M34860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alexey,&lt;/P&gt;&lt;P&gt;PTI1 (SCI1_TxD on pin #56) of the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MKM33Z128ACLH5 is designed as open drain to achieve 5V tolerance. It requires an external pull-up resistor for correct operation. As an external pull-up resistor, you can use an internal pull-up of the &lt;SPAN&gt;MK10DX256VLK7, that could be set on&amp;nbsp;&lt;SPAN style="color: #3d3d3d;"&gt;UART0&lt;/SPAN&gt;&lt;SPAN style="color: #3d3d3d;"&gt;_RxD (pin #35) operating in input mode. However, the weak internal pull-up of the MK10DX256VLK7 device might be limiting maximum communication data rate and therefore for achieving faster data rates and/or improving immunity of the communication line to external noises, you might still consider adding an external pull-up.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Kind regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN style="color: #3d3d3d;"&gt;Martin M.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 13:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pull-up-down-resistors-for-UART/m-p/594060#M34860</guid>
      <dc:creator>MarMi</dc:creator>
      <dc:date>2016-09-06T13:51:55Z</dc:date>
    </item>
  </channel>
</rss>