<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K64 Sub-Family Ref Manual -- type-O or EMAC Enhanaced Buff really change in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592608#M34823</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking closer -- looks like Offsets 8 and A also changed!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 19:10:22 GMT</pubDate>
    <dc:creator>JHinkle</dc:creator>
    <dc:date>2016-08-11T19:10:22Z</dc:date>
    <item>
      <title>K64 Sub-Family Ref Manual -- type-O or EMAC Enhanaced Buff really change</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592607#M34822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on a K64 EMET driver and compared the Enhanced Buffers between the K64 and the K60.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did the locations for the "Data Length" and the first set of status registers flip-flop, or is just a publication error?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K60 ................................................ Notice Offset 0 is Status flags&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="K60_EB.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1459i31879A7F22717D87/image-size/large?v=v2&amp;amp;px=999" role="button" title="K60_EB.png" alt="K60_EB.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K64 ..........................................................&amp;nbsp; Notice Offset 0 is Data Length&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="K64_EB.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1413iE909AEC315541403/image-size/large?v=v2&amp;amp;px=999" role="button" title="K64_EB.png" alt="K64_EB.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been running the K64 with the K60 layout and it seems to work but in tracking down an issue ... I noticed the flip-flop --- Which might be my issue if the actually did flip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 19:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592607#M34822</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-08-11T19:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: K64 Sub-Family Ref Manual -- type-O or EMAC Enhanaced Buff really change</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592608#M34823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking closer -- looks like Offsets 8 and A also changed!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 19:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592608#M34823</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-08-11T19:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: K64 Sub-Family Ref Manual -- type-O or EMAC Enhanaced Buff really change</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592609#M34824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a comment in K60 RM as follows just above the buffer descriptor description.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;NOTE&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;The following addresses are shown for a big endian implementation.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="TxBD NOTE.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1528i809D0262B0B9FF07/image-size/large?v=v2&amp;amp;px=999" role="button" title="TxBD NOTE.png" alt="TxBD NOTE.png" /&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually the module chapter is borrowed from original Coldfire device which is big endian architecture. When Kinetis (little endian) first introduce, the module chapter is not changed directly, just added a comment there. With later Kinetis device like K64/K65, associated information is updated and the comment removed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 01:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592609#M34824</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-08-15T01:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: K64 Sub-Family Ref Manual -- type-O or EMAC Enhanaced Buff really change</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592610#M34825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Robin:&lt;/P&gt;&lt;P&gt;Kinetis is a little endian device so why have documentation published that related to big endian.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess that means Kinetis users will have to be very careful when looking at published register assignments to verify if they are based on big/little endian configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for clarifying.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 14:12:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Sub-Family-Ref-Manual-type-O-or-EMAC-Enhanaced-Buff-really/m-p/592610#M34825</guid>
      <dc:creator>JHinkle</dc:creator>
      <dc:date>2016-08-15T14:12:10Z</dc:date>
    </item>
  </channel>
</rss>