<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK26 Overshoot acceptance</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K26-Overshoot-acceptance/m-p/592061#M34817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running Signal integrity simulation using K26 IBIS model and SDram device, but i am able to see overshoot at K26 for read condition So anybody tell me What is maximum overshoot acceptance for K26 device ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Aug 2016 06:46:26 GMT</pubDate>
    <dc:creator>pradeeppatil</dc:creator>
    <dc:date>2016-08-11T06:46:26Z</dc:date>
    <item>
      <title>K26 Overshoot acceptance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K26-Overshoot-acceptance/m-p/592061#M34817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running Signal integrity simulation using K26 IBIS model and SDram device, but i am able to see overshoot at K26 for read condition So anybody tell me What is maximum overshoot acceptance for K26 device ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 06:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K26-Overshoot-acceptance/m-p/592061#M34817</guid>
      <dc:creator>pradeeppatil</dc:creator>
      <dc:date>2016-08-11T06:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: K26 Overshoot acceptance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K26-Overshoot-acceptance/m-p/592062#M34818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you mean the voltage overshoot acceptance on the MCU input pins?&lt;/P&gt;&lt;P&gt;This is VDD+0.3V / VSS-0.3V&lt;/P&gt;&lt;P&gt;So if the VDD = 3.3V&lt;/P&gt;&lt;P&gt;Then the input signals should be in range -0.3V to 3.6V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Aug 2016 11:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K26-Overshoot-acceptance/m-p/592062#M34818</guid>
      <dc:creator>michael_galda</dc:creator>
      <dc:date>2016-08-11T11:20:56Z</dc:date>
    </item>
  </channel>
</rss>