<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Crash FlashCommandSequence without artificial delay</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Crash-FlashCommandSequence-without-artificial-delay/m-p/591819#M34815</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leif Zars,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to run the Flash driver demo which is from the KSDK 2.0 on your chip, and you can download the KSDK2.0 by referring to the thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329744" rel="nofollow noopener noreferrer" target="_blank"&gt;How to: install KSDK 2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And the KSDK2.0 also use the C90TFS/FTFxFlash Driver to execute the several kinds of the flash operation, however the flash_command_sequence() function can work well even without inserting the delay function. So it can help you to figure out the root cause of issue by compare the demo with your demo.&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_1467772210183870" data-renderedposition="138_8_1192_1040" jivemacro_uid="_1467772210183870" modifiedtitle="true"&gt;&lt;P&gt;/*!&lt;/P&gt;&lt;P&gt; * @brief Flash Command Sequence&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * This function is used to perform the command write sequence to the flash.&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * @param driver Pointer to storage for the driver runtime state.&lt;/P&gt;&lt;P&gt; * @return An error code or kStatus_FLASH_Success&lt;/P&gt;&lt;P&gt; */&lt;/P&gt;&lt;P&gt;static status_t flash_command_sequence(flash_config_t *config)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t registerValue;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if FLASH_DRIVER_IS_FLASH_RESIDENT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear RDCOLERR &amp;amp; ACCERR &amp;amp; FPVIOL flag in flash status register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_RDCOLERR_MASK | FTFx_FSTAT_ACCERR_MASK | FTFx_FSTAT_FPVIOL_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status_t returnCode = flash_check_execute_in_ram_function_info(config);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kStatus_FLASH_Success != returnCode)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return returnCode;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* We pass the ftfx_fstat address as a parameter to flash_run_comamnd() instead of using&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * pre-processed MICRO sentences or operating global variable in flash_run_comamnd()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * to make sure that flash_run_command() will be compiled into position-independent code (PIC). */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; callFlashRunCommand((FTFx_REG_ACCESS_TYPE)(&amp;amp;FTFx-&amp;gt;FSTAT));&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear RDCOLERR &amp;amp; ACCERR &amp;amp; FPVIOL flag in flash status register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_RDCOLERR_MASK | FTFx_FSTAT_ACCERR_MASK | FTFx_FSTAT_FPVIOL_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear CCIF bit */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_CCIF_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check CCIF bit of the flash status register, wait till it is set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * IP team indicates that this loop will always complete. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (!(FTFx-&amp;gt;FSTAT &amp;amp; FTFx_FSTAT_CCIF_MASK))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;#endif /* FLASH_DRIVER_IS_FLASH_RESIDENT */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check error bits */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Get flash status register value */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; registerValue = FTFx-&amp;gt;FSTAT;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking access error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (registerValue &amp;amp; FTFx_FSTAT_ACCERR_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_AccessError;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking protection error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if (registerValue &amp;amp; FTFx_FSTAT_FPVIOL_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_ProtectionViolation;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking MGSTAT0 non-correctable error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if (registerValue &amp;amp; FTFx_FSTAT_MGSTAT0_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_CommandFailure;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_Success;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jul 2016 02:31:47 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-07-06T02:31:47Z</dc:date>
    <item>
      <title>Crash FlashCommandSequence without artificial delay</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Crash-FlashCommandSequence-without-artificial-delay/m-p/591818#M34814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;C90TFS/FTFxFlash Driver&lt;/P&gt;&lt;P&gt;In function FlashCommandSequence the system hard faults. But when I add a delay everything works. Below notice the while loop with the nop, without it i get a hard fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using a K24FN1M0 using config FTFx_KX_(2048_1024)K_0K_(16_4)K_4K_0K.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_1467309354158660 jive_macro_code jive_text_macro" data-renderedposition="238_50_798_528" jivemacro_uid="_1467309354158660"&gt;&lt;P&gt;uint32_t SIZE_OPTIMIZATION FlashCommandSequence (PFLASH_SSD_CONFIG pSSDConfig )&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; disableISRs();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t ret;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* return code variable */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t temp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* temporary variable */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear CCIF to launch command */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp = pSSDConfig-&amp;gt;ftfxRegBase + FTFx_SSD_FSTAT_OFFSET;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; REG_BIT_SET(temp, FTFx_SSD_FSTAT_CCIF);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp = 1000000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(temp){&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm( "NOP" );&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp--;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* wait for completion of this command */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp = pSSDConfig-&amp;gt;ftfxRegBase + FTFx_SSD_FSTAT_OFFSET;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(0x0U == (REG_BIT_GET(temp, FTFx_SSD_FSTAT_CCIF)))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* wait till CCIF bit is set */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* serve callback function if counter reaches limitation */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(NULL_CALLBACK != pSSDConfig-&amp;gt;CallBack)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (pSSDConfig-&amp;gt;CallBack)();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; temp = pSSDConfig-&amp;gt;ftfxRegBase + FTFx_SSD_FSTAT_OFFSET;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ret = ((uint32_t)(REG_READ(temp)) &amp;amp; FTFx_SSD_FSTAT_ERROR_BITS);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; enableISRs();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return(ret);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 17:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Crash-FlashCommandSequence-without-artificial-delay/m-p/591818#M34814</guid>
      <dc:creator>leifzars</dc:creator>
      <dc:date>2016-06-30T17:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: Crash FlashCommandSequence without artificial delay</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Crash-FlashCommandSequence-without-artificial-delay/m-p/591819#M34815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leif Zars,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to run the Flash driver demo which is from the KSDK 2.0 on your chip, and you can download the KSDK2.0 by referring to the thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329744" rel="nofollow noopener noreferrer" target="_blank"&gt;How to: install KSDK 2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And the KSDK2.0 also use the C90TFS/FTFxFlash Driver to execute the several kinds of the flash operation, however the flash_command_sequence() function can work well even without inserting the delay function. So it can help you to figure out the root cause of issue by compare the demo with your demo.&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_1467772210183870" data-renderedposition="138_8_1192_1040" jivemacro_uid="_1467772210183870" modifiedtitle="true"&gt;&lt;P&gt;/*!&lt;/P&gt;&lt;P&gt; * @brief Flash Command Sequence&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * This function is used to perform the command write sequence to the flash.&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * @param driver Pointer to storage for the driver runtime state.&lt;/P&gt;&lt;P&gt; * @return An error code or kStatus_FLASH_Success&lt;/P&gt;&lt;P&gt; */&lt;/P&gt;&lt;P&gt;static status_t flash_command_sequence(flash_config_t *config)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t registerValue;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if FLASH_DRIVER_IS_FLASH_RESIDENT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear RDCOLERR &amp;amp; ACCERR &amp;amp; FPVIOL flag in flash status register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_RDCOLERR_MASK | FTFx_FSTAT_ACCERR_MASK | FTFx_FSTAT_FPVIOL_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status_t returnCode = flash_check_execute_in_ram_function_info(config);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (kStatus_FLASH_Success != returnCode)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return returnCode;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* We pass the ftfx_fstat address as a parameter to flash_run_comamnd() instead of using&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * pre-processed MICRO sentences or operating global variable in flash_run_comamnd()&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * to make sure that flash_run_command() will be compiled into position-independent code (PIC). */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; callFlashRunCommand((FTFx_REG_ACCESS_TYPE)(&amp;amp;FTFx-&amp;gt;FSTAT));&lt;/P&gt;&lt;P&gt;#else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear RDCOLERR &amp;amp; ACCERR &amp;amp; FPVIOL flag in flash status register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_RDCOLERR_MASK | FTFx_FSTAT_ACCERR_MASK | FTFx_FSTAT_FPVIOL_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* clear CCIF bit */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFx-&amp;gt;FSTAT = FTFx_FSTAT_CCIF_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check CCIF bit of the flash status register, wait till it is set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * IP team indicates that this loop will always complete. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (!(FTFx-&amp;gt;FSTAT &amp;amp; FTFx_FSTAT_CCIF_MASK))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;#endif /* FLASH_DRIVER_IS_FLASH_RESIDENT */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check error bits */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Get flash status register value */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; registerValue = FTFx-&amp;gt;FSTAT;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking access error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (registerValue &amp;amp; FTFx_FSTAT_ACCERR_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_AccessError;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking protection error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if (registerValue &amp;amp; FTFx_FSTAT_FPVIOL_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_ProtectionViolation;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* checking MGSTAT0 non-correctable error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if (registerValue &amp;amp; FTFx_FSTAT_MGSTAT0_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_CommandFailure;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kStatus_FLASH_Success;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 02:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Crash-FlashCommandSequence-without-artificial-delay/m-p/591819#M34815</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-06T02:31:47Z</dc:date>
    </item>
  </channel>
</rss>