<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックBLE on Hexiwear</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-on-Hexiwear/m-p/589749#M34727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a few question concerning the BLE function on the Hexiwear.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there an API or library for using the KW40z BLE SoC on the Hexiwear?&lt;/LI&gt;&lt;LI&gt;Is the BLE SoC's transmission being sent to a serial port or somewhere else?&lt;/LI&gt;&lt;LI&gt;Can the BLE send its data over the UART to a serial port?&lt;/LI&gt;&lt;LI&gt;Can you use a&amp;nbsp; programming language like Java to determine the BLE RSSI from the Hexiwear? If not, can the Hexiwear determine its own RSSI with the paired device?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thank you in advance for helping me!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Sep 2016 16:55:28 GMT</pubDate>
    <dc:creator>microbob</dc:creator>
    <dc:date>2016-09-03T16:55:28Z</dc:date>
    <item>
      <title>BLE on Hexiwear</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-on-Hexiwear/m-p/589749#M34727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have a few question concerning the BLE function on the Hexiwear.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there an API or library for using the KW40z BLE SoC on the Hexiwear?&lt;/LI&gt;&lt;LI&gt;Is the BLE SoC's transmission being sent to a serial port or somewhere else?&lt;/LI&gt;&lt;LI&gt;Can the BLE send its data over the UART to a serial port?&lt;/LI&gt;&lt;LI&gt;Can you use a&amp;nbsp; programming language like Java to determine the BLE RSSI from the Hexiwear? If not, can the Hexiwear determine its own RSSI with the paired device?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thank you in advance for helping me!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Sep 2016 16:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/BLE-on-Hexiwear/m-p/589749#M34727</guid>
      <dc:creator>microbob</dc:creator>
      <dc:date>2016-09-03T16:55:28Z</dc:date>
    </item>
  </channel>
</rss>