<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL02 Min Max Input Current Voltage</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588887#M34685</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL02 chip includes four pins, PTB0, PTB1, PTA12, and PTA13, with high current drive capability. These pins can be used to drive LED or power MOSFET directly. So, those four pins could tolerance input current up to 20mA.&lt;/P&gt;&lt;P&gt;The KL02 chip includes two pins, PTB3 and PTB4, with true open drain setting. These pins have the capability to support 5 V voltage input in 3.3 V systems. Those pins could tolerance input current Max. value is 5mA.&lt;/P&gt;&lt;P&gt;The other IO pins are normal drive pin, which input current Max. value is 5mA.&lt;/P&gt;&lt;P&gt;In general, after reset, the digital IO pins go to a disabled (high impedance) state. So if the input voltage doesn't exceed the operation range (Max. 3.6V), there doesn't generate damage current.&lt;/P&gt;&lt;P&gt;The pins with analog functionality will default to their analog functions. If the input voltage doesn't exceed the operation range (Max. 3.6V), the analog pin could not be damaged.&lt;/P&gt;&lt;P&gt;The previous mentioned input current is available, when the related pin configured as GPIO input function.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Sep 2016 04:28:29 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-09-14T04:28:29Z</dc:date>
    <item>
      <title>KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588870#M34668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a design where I need the KL02 input ESD protection to clamp the input signal.&amp;nbsp; I can limit the input signal current using a resistor, but the voltage may be up to +/-25 V.&amp;nbsp; I have read the datasheet (KL02P32M48SF0 rev4 08/2014) and saw page 7 which said:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;All I/O pins are internally clamped to VSS through a ESD protection diode. There is no diode connection to VDD. If VIN greater than VIO_MIN (= VSS-0.3 V) is observed, then there is no need to provide current limiting resistors at the pads. If this limit cannot be observed then a current limiting resistor is required. The negative DC injection current limiting resistor is calculated as R = (VIO_MIN - VIN)/| IICIO| .&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But this only discusses negative voltage and current, not positive.&amp;nbsp; In addition, the above states there is no diode connection to VDD, so presumably there is a different ESD structure to limit positive ESD events.&amp;nbsp; Is it adequate to limit the positive current to the same value of | Iicio | = 3 mA?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 19:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588870#M34668</guid>
      <dc:creator>marky</dc:creator>
      <dc:date>2016-09-02T19:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588871#M34669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend customer to refer below thread about input injection current:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'Microsoft Yahei'; font-size: 14px; font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: 21px; orphans: auto; text-align: left; text-indent: -36px; text-transform: none; white-space: normal; widows: 1; word-spacing: 0px; -webkit-text-stroke-width: 0px; display: inline !important; float: none; background-color: #ffffff;"&gt;To Kinetis product, the DC injection current is +/-5mA.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/433880" target="_blank"&gt;https://community.nxp.com/thread/433880&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Sep 2016 03:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588871#M34669</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-05T03:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588872#M34670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do all Kinetis product have the same DC injection current?&amp;nbsp; Although KL03 datasheet states 5 mA, I am using KL02.&amp;nbsp; KL02 datasheet (KL02P32M48SF0 rev4 08/2014) states 3 mA.&amp;nbsp; Note that these are negative voltages and currents, whereas my questions is about positive voltages and currents.&amp;nbsp; Perhaps the other referenced thread about input injection current helps, but I could not find the referenced thread.&amp;nbsp; The above link loops back to this thread.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Sep 2016 13:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588872#M34670</guid>
      <dc:creator>marky</dc:creator>
      <dc:date>2016-09-05T13:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588873#M34671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As per the paragraph you quoted, there is NO diode-tie to VDD.&amp;nbsp; You must externally insure the pin voltage does not exceed the input-max (breakdown) voltage, such as by your OWN diode -- but note that with that plan you must insure the VDD-load is always greater than the max possible positive injection current from all sources. Another option is a shunt-regulator diode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is NOT a 'current injection' issue for these voltage-tolerant GPIO input-mode pins relating to the Kinetis chip itself.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 03:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588873#M34671</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-06T03:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588874#M34672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Earl, you addressed my question though it is not the answer I was hoping for.&amp;nbsp; The IO pin input voltage (VIO) is rated -0.3 to VDD + 0.3 V.&amp;nbsp; And yet the ESD rating is +/-500 and +/-2000 V.&amp;nbsp; There must be an on-chip structure for +V ESD events that performs some clamping and can absorb some energy.&amp;nbsp; But doing what you say and limiting the input voltage to VDD + 0.3 V using additional components is certainly safe and reasonable.&amp;nbsp; Finding the board space is the hard part.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 13:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588874#M34672</guid>
      <dc:creator>marky</dc:creator>
      <dc:date>2016-09-06T13:43:30Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588875#M34673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have to agree that the statements 'No diode to Vdd' and 'max Vdd+0.3" are incongruous.&amp;nbsp; On parts that specifically tout 5V-tolerance on I/O (looking at K60-100 for instance) the Vih(max) is given as 5.5V, independent from Vdd (on pins with such tolerance, does not apply to all digital I/O).&amp;nbsp; And for such part the injection current is given only as -5mA for such pins, but also listed is +/-5mA for clamped pins (analog-capable, reset, crystal) -- plus the 'regional limits'.&amp;nbsp; I think NXP will have to clarify the KL I/O structures for you!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 21:07:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588875#M34673</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-06T21:07:07Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588876#M34674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for previous incorrect link address, correct link is :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/432843"&gt;https://community.nxp.com/thread/432843&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no diode tie to VDD, which direct tie to the internal ESD bus.&lt;/P&gt;&lt;P&gt;The pad input voltage should not exceed the KL02 datasheet showed 3.6V.&lt;/P&gt;&lt;P&gt;The negative DC inject current is -3mA is clamped VSS ESD protection diode spec requirement.&lt;/P&gt;&lt;P&gt;Obviously, there is no DC inject current data for clamped VDD ESD protection diode.&lt;/P&gt;&lt;P&gt;My previous mentioned Kinetis product DC injection current is for Kinetis K family product.&lt;/P&gt;&lt;P&gt;Sorry for bring the confusion.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 03:09:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588876#M34674</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-07T03:09:25Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588877#M34675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, but that is exactly the point here -- the KL02 datasheet DOESN'T say Vin(max) 3.6V, it says Vdd+0.3 (Table 4 of section 1.4, Vio Min./Max.), and Vdd absolute-max 3.8V.&amp;nbsp; The 'Vdd +0.3V' requirement doesn't make any SENSE if there IS no explicit or implicit diode-clamp to Vdd on the digital-only I/O pins.&amp;nbsp; I would expect such pins to specifically list a fixed Vin(max) based on breakdown, as did the K60-100.&amp;nbsp; If that is indeed 3.6V, then so be it -- but isn't 3.8V+0.3V=4.1V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 12:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588877#M34675</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-07T12:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588878#M34676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;General advice is great for people that need it, but I was hoping for specifics.&amp;nbsp; The IO pins obviously have circuitry to deal with positive transients like ESD.&amp;nbsp; This circuitry must do some clamping and must be able to absorb some energy.&amp;nbsp; Unfortunately, NXP does not provide any useful information in utilizing this circuitry in a a safe and reliable manner.&amp;nbsp; "Don't use it" is of course safe and reliable but adds potentially unnecessary cost and board space to a design.&amp;nbsp; In the interests of the community I provide some quick measurements on a KL02Z32 on pin PTA11 with the part powered and the pin connected to a variable voltage supply with a 1 MOhm current limiting resistor.&amp;nbsp; All following values are approximate and just one part, room temp, etc etc.&amp;nbsp; The pin's voltage was 5.2V at 1uA input current, 6.1V at 10uA, and 6.4V at 20 uA.&amp;nbsp; I suspect the input structure is similar or identical to 5V tolerant parts.&amp;nbsp; However, this part is &lt;SPAN style="text-decoration: underline;"&gt;not&lt;/SPAN&gt; specified for 5V inputs, perhaps because that would require additional cost for production testing, perhaps because process controls would need to be tighter or yields would be lower, or perhaps other reasons.&amp;nbsp; Again, utilizing this circuitry could be useful in some designs, but doing so is at the user's risk with no promises or even design information available from NXP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 16:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588878#M34676</guid>
      <dc:creator>marky</dc:creator>
      <dc:date>2016-09-07T16:41:59Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588879#M34677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for those actual measurements!&amp;nbsp; They further underscore a requirement for NXP to clarify the voltage-tolerance on 'presumably' that set of pins NOT analog-capable, or RESET or Crystal, and then fix this (and MOST KL datasheets!) relative to these requirements!&amp;nbsp; KL02 and KL03 datasheets seem to have the limitations we have discussed here -- KL04 does show minus AND PLUS clamp currents, BUT Iicio in Table 5 for 'positive injection current' shows +current for Vin &amp;lt; Vss-0.3, as copied from 'negative injection' -- a minor typo....&amp;nbsp; The KL05 Table-1 numbers make sense, although 'note 1' only mentions dual-clamp-diodes relative to analog pins -- I should expect it applies to ALL I/O pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 18:28:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588879#M34677</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-07T18:28:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588880#M34678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL02 datasheet table 4 voltage and current operation ratings VIO value is the IO pin could tolerance ultimate max. voltage up to 4.1V. While, this value is instantaneous Max. tolerance input voltage value, not the long-term normally working Max. input voltage value. Customer need to refer Table 5 for voltage operating requirements for long-term working IO pin input voltage need below Max. value 3.6V.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 01:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588880#M34678</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-08T01:57:01Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588881#M34679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know what datasheet YOU are looking at -- the newest KL02 I can find on the NXP web is dated 8/2014 (Rev 4, KL02P20M48SF0.pdf.&amp;nbsp; Same date/rev/info for KL02P32M48SF0.pdf), and for those two years these datasheets have shown these errors and omissions.&amp;nbsp; Table 5 does NOT give ANY positive voltage limit information on Vin, ONLY on Vdd, AND Vin &lt;SPAN style="text-decoration: underline;"&gt;threshold&lt;/SPAN&gt;-information based on Vdd ranges.&amp;nbsp; The 4.1V I posited 'from Table 4' is a simple calculation of the two voltage parameters there, but is based on the VERY FLAWED PREMISE that the IO pin voltage is limited by a Vdd +0.3 clamp, which actual measurements have PROVEN to be INCORRECT --- note 1 of Table 5 &lt;SPAN style="text-decoration: underline;"&gt;IS&lt;/SPAN&gt; correct in that there IS no direct clamp to Vdd.&amp;nbsp; And I AGREE that any inference from Table 4 is an 'absolute max', NOT an 'operating level'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ideally NXP would fix the datasheets and release new revisions, for (at least!) ALL the KL0x devices, to clear up the errors, omissions, and ambiguous information regarding the input structure specifications for max Vih --- or at LEAST release datasheet errata.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 12:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588881#M34679</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-08T12:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588882#M34680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the support.&amp;nbsp; Personally, I would not describe the datasheets as incorrect, but rather overly conservative and not as complete as we would like.&amp;nbsp; General comments as a first time user of a Kinetis uC:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Table 4 is labeled "Voltage and current operating ratings".&amp;nbsp; Most companies call this something like "Absolute Maximum Ratings".&amp;nbsp; After all, Table 4 says the supply voltage can be -0.3 to 3.8 V, but the part will definitely not be operational powered at -0.3 V.&amp;nbsp; Some companies put a note for this table regarding the part is not necessarily operational (functional), won't be damaged by short-term exposure to these levels, but may be damaged by long-term exposure.&lt;/LI&gt;&lt;LI&gt;Table 4's VIO input pin voltage minimum of -0.3 V shouldn't be taken literally since Table 5 indicates this can be exceeded (more negative than -0.3 V) if the current is limited.&amp;nbsp; Of course the whole point of this discussion topic is to have similar information for exceeding the positive limit in Table 4.&lt;/LI&gt;&lt;LI&gt;Table 3 has ESD ratings.&amp;nbsp; This table indicates the part will not be damaged by transient voltages that are orders of magnitude higher than the voltages in Table 4.&amp;nbsp; My interest for my design is regarding non-ESD transients.&amp;nbsp; Without getting further information from NXP, I may look at the test conditions in the ESD standards, calculate the amount of discharge energy, safety factor the energy down by a factor of 3 to 10, then use that value to choose a current-limiting resistor for positive transients.&amp;nbsp; Ideally, manufacturers would provide max currents, voltages and/or energies with durations from DC to nanoseconds.&amp;nbsp; Some passive component manufacturers do this (resistors for example).&amp;nbsp; This would be useful information for the customer using the part, but the time/effort on the supplier's side is significant.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am asking what maximum positive current or energy can safely be applied to an IO pin without causing damage and/or without causing a functional issue.&amp;nbsp; The part's ESD structure clearly can handle some level of current and energy, and I would like to take advantage of it.&amp;nbsp; Since the NXP answer so far is basically "don't utilize the part's ESD structure" by limiting the positive voltage to VDD+0.3V, I consider my question still unanswered.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 14:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588882#M34680</guid>
      <dc:creator>marky</dc:creator>
      <dc:date>2016-09-08T14:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588883#M34681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are checking the same datasheet.&lt;/P&gt;&lt;P&gt;Yes, I do agree with you about the KL product datasheet issue. There should with more explicit data about related IO pin input voltage. The datasheet should show more detailed info, not just bring confusion.&lt;/P&gt;&lt;P&gt;I will pass related voice to the Kinetis L product team.&lt;/P&gt;&lt;P&gt;Thank you for the input, I really appreciate that feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with regards,&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 09:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588883#M34681</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-09T09:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588884#M34682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will check with Kinetis L product team about your required data.&lt;/P&gt;&lt;P&gt;I will let you know when there with any feedback.&lt;/P&gt;&lt;P&gt;Thank you for the patience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 09:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588884#M34682</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-09T09:25:36Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588885#M34683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the patience.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the KL02 product standard I/O pin(normal drive pad), the Max. positive current is 5mA;&lt;/P&gt;&lt;P&gt;The High drive pad, the Max. positive current is 20mA.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 07:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588885#M34683</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-13T07:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588886#M34684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nice information -- but what does DRIVE CURRENT have to do with input-voltage-withstand in 'input mode'????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 13:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588886#M34684</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-13T13:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588887#M34685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL02 chip includes four pins, PTB0, PTB1, PTA12, and PTA13, with high current drive capability. These pins can be used to drive LED or power MOSFET directly. So, those four pins could tolerance input current up to 20mA.&lt;/P&gt;&lt;P&gt;The KL02 chip includes two pins, PTB3 and PTB4, with true open drain setting. These pins have the capability to support 5 V voltage input in 3.3 V systems. Those pins could tolerance input current Max. value is 5mA.&lt;/P&gt;&lt;P&gt;The other IO pins are normal drive pin, which input current Max. value is 5mA.&lt;/P&gt;&lt;P&gt;In general, after reset, the digital IO pins go to a disabled (high impedance) state. So if the input voltage doesn't exceed the operation range (Max. 3.6V), there doesn't generate damage current.&lt;/P&gt;&lt;P&gt;The pins with analog functionality will default to their analog functions. If the input voltage doesn't exceed the operation range (Max. 3.6V), the analog pin could not be damaged.&lt;/P&gt;&lt;P&gt;The previous mentioned input current is available, when the related pin configured as GPIO input function.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 04:28:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588887#M34685</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-14T04:28:29Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588888#M34686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ignoring the information about drive-power-level, as in 'high impedance' state that is certainly completely irrelevant.&amp;nbsp; I would like to know where you get a SPEC for 5V-tolerance on PTB3 and PTB4, and where you get the 3.6V-max rating for all other digital input pins!&amp;nbsp; Given the voltage-input measurements Marky made, I assure you there is NO WAY to 'shove' 5 or 20mA INTO an input-mode pin!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 11:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588888#M34686</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-14T11:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Min Max Input Current Voltage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588889#M34687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Despite your measurements, with 'no available information to the contrary' I suppose you will have to take the 'safe option' and limit, with hardware, such pins to &amp;lt; (Vdd+0.3V).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Sep 2016 18:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Min-Max-Input-Current-Voltage/m-p/588889#M34687</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-09-14T18:11:35Z</dc:date>
    </item>
  </channel>
</rss>