<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K82F , bootloader device does not appear in win 7 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588713#M34648</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;Yes, as the thread &lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-content-finding="Community" data-objectid="100720" data-objecttype="102" href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt; states, the OpenSDA 2.0 &amp;amp; 2.1 both are open source, so the K82 and K20 both can be programmed and the JTAG or SWD interface mode both are available.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 07:55:16 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-07-20T07:55:16Z</dc:date>
    <item>
      <title>FRDM-K82F , bootloader device does not appear in win 7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588710#M34645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I bought a couple of these boards. One of them worked correctly&amp;nbsp; after switching to firmware "JLink_OpenSDA_V2_1_2015-10-13.bin" . I can see the device in the device manager, and can program it via Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to setup the second board, by starting it as bootloader (RESET button). I was able to see the BOOTLOADER drive, and then I flashed the above-mentioned firmware. However, this time I briefly saw a message stating that the file was too big (or the space was too small?). The device disappears, and I cannot get it to show up again. No BOOTLOADER, no OPENSDA device either. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ideas from the back of my memory:&lt;/P&gt;&lt;P&gt;a)&amp;nbsp; While trying to get the first board up and running, I recall having tried to flash a different firmware, as in some site I read that openSDA2.1 would not fit in the memory allocated by the original P&amp;amp;E firmware. Which one did I flash? I do not remember, but it could be one of the following, based on the files that I still have on my disk:&lt;/P&gt;&lt;P&gt;- 04_OpenSDA_FRDM-K82F.bin&lt;/P&gt;&lt;P&gt;- JLink_OpenSDA_V2_1.bin&lt;/P&gt;&lt;P&gt;- OpenSDA_V2_1.bin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is there a specific order in which the firmware needs to be updated? The board was originally showing as an MBED device.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;b) I can program the K82 using J11 and the flashing tool. This seems to be no problem. However, I would like to get the K20 up and running again. I saw in another post that there is a bin file for the K20 that is mounted on the same board. The quesiton is, how to get it in there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is there a way to program the K20 without having access to a JTAG debugger? E.g. by programming via the K82, or something else?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for the help. I hope my that my board is done for :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 15:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588710#M34645</guid>
      <dc:creator>javiersoriano</dc:creator>
      <dc:date>2016-07-19T15:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F , bootloader device does not appear in win 7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588711#M34646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;a)&amp;nbsp; While trying to get the first board up and running, I recall having tried to flash a different firmware, as in some site I read that openSDA2.1 would not fit in the memory allocated by the original P&amp;amp;E firmware. Which one did I flash? I do not remember, but it could be one of the following, based on the files that I still have on my disk:&lt;/P&gt;&lt;P&gt;- 04_OpenSDA_FRDM-K82F.bin&lt;/P&gt;&lt;P&gt;- JLink_OpenSDA_V2_1.bin&lt;/P&gt;&lt;P&gt;- OpenSDA_V2_1.bin&lt;/P&gt;&lt;P&gt;-- I've try all those firmware, they all can makes the OpenSDA compatible to J-Link lite.&amp;nbsp; And I've attached all those firmware.&lt;/P&gt;&lt;P&gt;b) I can program the K82 using J11 and the flashing tool. This seems to be no problem. However, I would like to get the K20 up and running again. I saw in another post that there is a bin file for the K20 that is mounted on the same board. The quesiton is, how to get it in there?&lt;/P&gt;&lt;P&gt;-- Of course, you can program the K82 directly through the J9, and the J19 is for the K20.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can learn the more information from the thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 02:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588711#M34646</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-20T02:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F , bootloader device does not appear in win 7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588712#M34647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply and the files. I am assuming that you got all of these working by copying the file into the device that is mounted as a USB drive (BOOTLOADER)? My problem is that I cannot see that device anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you mention J9, and J19, I assume also that you mean they can be programmed via JTAG. At the moment I do not have access to one, I will look around to find out which model I need to do so. (Any pointers are appreciated)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Javier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 07:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588712#M34647</guid>
      <dc:creator>javiersoriano</dc:creator>
      <dc:date>2016-07-20T07:41:26Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F , bootloader device does not appear in win 7</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588713#M34648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;Yes, as the thread &lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-content-finding="Community" data-objectid="100720" data-objecttype="102" href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt; states, the OpenSDA 2.0 &amp;amp; 2.1 both are open source, so the K82 and K20 both can be programmed and the JTAG or SWD interface mode both are available.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 07:55:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K82F-bootloader-device-does-not-appear-in-win-7/m-p/588713#M34648</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-20T07:55:16Z</dc:date>
    </item>
  </channel>
</rss>