<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MKL03 in-software flash programming in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587593#M34616</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please,can you specify wich are the right and the bad clock configurations?Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 06:19:22 GMT</pubDate>
    <dc:creator>diegocolombo</dc:creator>
    <dc:date>2018-08-16T06:19:22Z</dc:date>
    <item>
      <title>MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587590#M34613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to re-flash few sectors of MKL03 internal flash in software.&amp;nbsp; When I run the flash_example out of the SDK1.3 example drivers, the flash sectors are programmed correctly.&amp;nbsp; However, when I add the flash component to my project through Processor Expert, and I try to use the same logic as the example, the desired sectors are not being flashed.&amp;nbsp; I already checked that the flash configuration is done correctly and my FlashCommandSequence function is relocated to RAM, but its execution does not change the content of the flash.&amp;nbsp; Are there any other settings (power, clk, etc.) that I need to change in order to get the re-flashing working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 13:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587590#M34613</guid>
      <dc:creator>arturzak</dc:creator>
      <dc:date>2016-07-19T13:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587591#M34614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can't write the data to the flash, did you meet any problem when debug it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you disable the interrupt before you do the flash operation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can refer to this post at first, make sure you disable the global interrupt:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/597793#comment-597793" title="https://community.nxp.com/message/597793#comment-597793"&gt;https://community.nxp.com/message/597793&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The code you can refer to the KSDK1.3.0 flash demo.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 06:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587591#M34614</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-07-20T06:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587592#M34615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jingjing,&lt;/P&gt;&lt;P&gt;I was able to resolve my issue.&amp;nbsp; In addition to disabling global interrupts, I had to re-configure my my clock configuration with proper Bus/Flash clock.&amp;nbsp; Once I had the clock correct, I was able to in-software program the internal flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 13:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587592#M34615</guid>
      <dc:creator>arturzak</dc:creator>
      <dc:date>2016-07-20T13:41:50Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587593#M34616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please,can you specify wich are the right and the bad clock configurations?Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 06:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587593#M34616</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2018-08-16T06:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587594#M34617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Diego,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you have the KL03 problem, please create your own question post, we will help you in your own post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 09:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587594#M34617</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-08-16T09:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: MKL03 in-software flash programming</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587595#M34618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Kerry Zhou,&lt;/P&gt;&lt;P&gt;i already did it but i 'm even more confused&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/478394"&gt;https://community.nxp.com/thread/478394&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;Best regards&lt;BR /&gt;Diego&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 12:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL03-in-software-flash-programming/m-p/587595#M34618</guid>
      <dc:creator>diegocolombo</dc:creator>
      <dc:date>2018-08-16T12:00:46Z</dc:date>
    </item>
  </channel>
</rss>