<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Can't debug an application in KDS with Segger j-link</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-debug-an-application-in-KDS-with-Segger-j-link/m-p/586461#M34589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jenia Brook&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you change the start address of you LED Blink program to work with you bootloader?&lt;/P&gt;&lt;P&gt;If so, maybe you are having the same issue that this post: &lt;A href="https://community.nxp.com/thread/391092"&gt;Debugging Application in KDS with Bootloader&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to check it and tell me if you have any question&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 15:13:20 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2016-07-20T15:13:20Z</dc:date>
    <item>
      <title>Can't debug an application in KDS with Segger j-link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-debug-an-application-in-KDS-with-Segger-j-link/m-p/586460#M34588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've a problem to debug the code on &lt;STRONG&gt;KE04Z128&lt;/STRONG&gt; (Not on evaluation board). It just seems to be stuck, not even stops at the beginning of main() function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It used to work good, I have some LED Blink program that worked good, until I started to implement Serial Bootloader (accordingly to AN4767 document) on that micro-controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First of all the Serial Bootloader was implemented on &lt;SPAN style="text-decoration: underline;"&gt;&lt;SPAN style="color: #606060; text-decoration: underline;"&gt;FRDM-KE06Z evaluation board&lt;/SPAN&gt;&lt;/SPAN&gt; and it worked great, I've been able to upload a S19 (srec) file through the AN2295 PC to the FRDM-KE06Z and verified that it worked as it should be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that I've started to implement the bootloader on &lt;STRONG&gt;KE04Z128&lt;/STRONG&gt;. The communications through UART (RS485) between the AN2295 PC and the target is good, I can erase addresses (from 0x4000 to end of flash --&amp;gt; 0x4000 is where my app should start) but not be able to program (another story...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I decided go back to the LED Blink program, and now as I said before, I can't debug it.&lt;/P&gt;&lt;P&gt;I've opened a new project and write another LED Blink program, still no result, it stuck.&lt;/P&gt;&lt;P&gt;When I go back to bootloader project I &lt;STRONG&gt;can&lt;/STRONG&gt; debug it. Other projects I can't debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know what seems to be a problem and from where to begin to solve this annoying issue.&lt;/P&gt;&lt;P&gt;Is anyone could guide me through?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Jenia&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 09:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-debug-an-application-in-KDS-with-Segger-j-link/m-p/586460#M34588</guid>
      <dc:creator>jeniabrook</dc:creator>
      <dc:date>2016-07-19T09:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can't debug an application in KDS with Segger j-link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-debug-an-application-in-KDS-with-Segger-j-link/m-p/586461#M34589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jenia Brook&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you change the start address of you LED Blink program to work with you bootloader?&lt;/P&gt;&lt;P&gt;If so, maybe you are having the same issue that this post: &lt;A href="https://community.nxp.com/thread/391092"&gt;Debugging Application in KDS with Bootloader&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you to check it and tell me if you have any question&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 15:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-debug-an-application-in-KDS-with-Segger-j-link/m-p/586461#M34589</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-07-20T15:13:20Z</dc:date>
    </item>
  </channel>
</rss>