<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN_LDD configuration on MK64FN1M0VLL12 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585584#M34554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, got the driver send the acknowledge bit during transmission. From this I know that the HW portion is working.&lt;/P&gt;&lt;P&gt;However the RxTxInterrupt is never triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also executing the SendFrame method doesn't have any effect on the bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for any advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 09:29:18 GMT</pubDate>
    <dc:creator>tommyb90</dc:creator>
    <dc:date>2016-09-06T09:29:18Z</dc:date>
    <item>
      <title>CAN_LDD configuration on MK64FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585583#M34553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm having issues configuring the CAN bus controller on the MK64F Microcontroller.&lt;/P&gt;&lt;P&gt;I use a FRDM-KE06 to send data over a CAN bus (tested and working on another circuit) and I have to receive data on a&amp;nbsp;MK64FN1M0VLL12 mounted on a custom circuit, the CAN adapter is an MCP2551.&lt;/P&gt;&lt;P&gt;As I try to send data over the bus from the MK64F, no signal is transmitted.&lt;/P&gt;&lt;P&gt;If I transmit from the KE06, I can see data is transmitted, but not received from the K64F and the RxInterrupt is never called.&lt;/P&gt;&lt;P&gt;The configuration is the same and I keep the same component in both cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 13:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585583#M34553</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2016-09-02T13:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_LDD configuration on MK64FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585584#M34554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, got the driver send the acknowledge bit during transmission. From this I know that the HW portion is working.&lt;/P&gt;&lt;P&gt;However the RxTxInterrupt is never triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also executing the SendFrame method doesn't have any effect on the bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for any advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 09:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585584#M34554</guid>
      <dc:creator>tommyb90</dc:creator>
      <dc:date>2016-09-06T09:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_LDD configuration on MK64FN1M0VLL12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585585#M34555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend customer to refer CAN_LDD component example located at CodeWarrior V10.6 installation path(below is default path):&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K60N512\CAN&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 05:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CAN-LDD-configuration-on-MK64FN1M0VLL12/m-p/585585#M34555</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-09-07T05:54:48Z</dc:date>
    </item>
  </channel>
</rss>