<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MK20DX128VLH7 has FlexBus or not? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX128VLH7-has-FlexBus-or-not/m-p/584816#M34540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im designing a board with the MK20DXxxxVLH7 mcu's (64 pin K20).&amp;nbsp; The datasheet and reference guide list all the Flexbus pins as ALT5 on the pinout.&amp;nbsp; BUT the reference guide and Datasheet have no mention of Flexbus.&amp;nbsp; So my question is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are the FlexBus pins documented on function ALT5 in both manuals incorrect and the part has no Flexbus?&lt;/P&gt;&lt;P&gt;OR&lt;/P&gt;&lt;P&gt;Are both manuals inadvertently omitting data on the Flexbus interface in the 64 pin K20?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 01:59:22 GMT</pubDate>
    <dc:creator>stevenjohnson</dc:creator>
    <dc:date>2016-07-19T01:59:22Z</dc:date>
    <item>
      <title>MK20DX128VLH7 has FlexBus or not?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX128VLH7-has-FlexBus-or-not/m-p/584816#M34540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im designing a board with the MK20DXxxxVLH7 mcu's (64 pin K20).&amp;nbsp; The datasheet and reference guide list all the Flexbus pins as ALT5 on the pinout.&amp;nbsp; BUT the reference guide and Datasheet have no mention of Flexbus.&amp;nbsp; So my question is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are the FlexBus pins documented on function ALT5 in both manuals incorrect and the part has no Flexbus?&lt;/P&gt;&lt;P&gt;OR&lt;/P&gt;&lt;P&gt;Are both manuals inadvertently omitting data on the Flexbus interface in the 64 pin K20?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 01:59:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX128VLH7-has-FlexBus-or-not/m-p/584816#M34540</guid>
      <dc:creator>stevenjohnson</dc:creator>
      <dc:date>2016-07-19T01:59:22Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DX128VLH7 has FlexBus or not?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX128VLH7-has-FlexBus-or-not/m-p/584817#M34541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;K20&lt;/SPAN&gt; 64LQFP package products has &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;Flexbus&lt;/SPAN&gt; module.The datasheet or reference manual for this package had this feature missed, sorry. Customer should refer to other package &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;K20&lt;/SPAN&gt; 72MHz product(such as 100pins) documents for &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;Flexbus&lt;/SPAN&gt; related description. Sorry for the confusion this had caused.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 08:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX128VLH7-has-FlexBus-or-not/m-p/584817#M34541</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-07-19T08:19:30Z</dc:date>
    </item>
  </channel>
</rss>