<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: S9KEAZN8AMFK Exposed Pad Connection Problems</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582089#M34410</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZhongYao,&lt;/P&gt;&lt;P&gt;The RESET_b pin, if enabled, must have a 100 nF capacitor close to the MCU for transient protection. The NMI_b pin, if enabled, must not have any capacitance connected to it. Each pin, when enabled as their default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reset, the shared peripheral functions are disabled so that the pins are controlled by the parallel I/O except PTA4, PTA0, PTB4 and PTA5 that are default to SWD_DIO, SWD_CLK, NMI and RESET function. Driving the NMI signal low forces a non-maskable interrupt, if the NMI function is selected on the corresponding pin.&lt;/P&gt;&lt;P&gt;If you hope the PTB4(deault as NMI_b function) as SPI0_MISO, please modify the NMIE bit in SIM_SOPT register first.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60545iD26A433EABE86FB5/image-size/large?v=v2&amp;amp;px=999" title="NMIE.png" alt="NMIE.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can configure PTB1 as SPI0_MISO function instead of using PTB4(NMI_b).&lt;/P&gt;&lt;P&gt;Then configure PTA3 as UART0_TX and PTA2 as UART0_RX. (Please note that PTA2 and PTA3 are true open-drain pins when operated as output.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want use the debugger on FRDM-KEAZ128, please isolate the on-board MCU from the debug interface. (for example don't use the R101)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2016 09:33:16 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2016-06-28T09:33:16Z</dc:date>
    <item>
      <title>S9KEAZN8AMFK Exposed Pad Connection Problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582088#M34409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am use FRDM-KEAZ128Q80 as OpenOCD debugger, and it works well on a S9KEAZ128AMLH chip. but when I try to debug a S9KEAZN8AMFK mcu ,It doesn't work. It can't reconize the mcu.&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have connected the Exposed Pad to the ground, I searched the &amp;lt;KEA8 Sub-Family Reference Manual&amp;gt; but I don't found how to deal with the Exposed Pad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My schematic has been attached. *Note that I have been conncted the Exposed Pad to the ground. &lt;/P&gt;&lt;P&gt;I tested the pin PTA5/RESET voltage is 2.8v , it is very strange. help me please .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 07:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582088#M34409</guid>
      <dc:creator>54anson</dc:creator>
      <dc:date>2016-06-28T07:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN8AMFK Exposed Pad Connection Problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582089#M34410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZhongYao,&lt;/P&gt;&lt;P&gt;The RESET_b pin, if enabled, must have a 100 nF capacitor close to the MCU for transient protection. The NMI_b pin, if enabled, must not have any capacitance connected to it. Each pin, when enabled as their default function, has a weak internal pullup, but an external 4.7 kΩ to 10 kΩ pullup is recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After reset, the shared peripheral functions are disabled so that the pins are controlled by the parallel I/O except PTA4, PTA0, PTB4 and PTA5 that are default to SWD_DIO, SWD_CLK, NMI and RESET function. Driving the NMI signal low forces a non-maskable interrupt, if the NMI function is selected on the corresponding pin.&lt;/P&gt;&lt;P&gt;If you hope the PTB4(deault as NMI_b function) as SPI0_MISO, please modify the NMIE bit in SIM_SOPT register first.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60545iD26A433EABE86FB5/image-size/large?v=v2&amp;amp;px=999" title="NMIE.png" alt="NMIE.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can configure PTB1 as SPI0_MISO function instead of using PTB4(NMI_b).&lt;/P&gt;&lt;P&gt;Then configure PTA3 as UART0_TX and PTA2 as UART0_RX. (Please note that PTA2 and PTA3 are true open-drain pins when operated as output.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want use the debugger on FRDM-KEAZ128, please isolate the on-board MCU from the debug interface. (for example don't use the R101)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 09:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582089#M34410</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-06-28T09:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN8AMFK Exposed Pad Connection Problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582090#M34411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks to Robin, problems has been solved. These problems cased by NMI_b pin connection, I cut the NMI_b wire on my pcb then it could be recognized by J-Link.&amp;nbsp;&amp;nbsp; Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 08:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/582090#M34411</guid>
      <dc:creator>54anson</dc:creator>
      <dc:date>2016-06-30T08:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: S9KEAZN8AMFK Exposed Pad Connection Problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/1724514#M65549</link>
      <description>&lt;P&gt;Hi Robin&lt;/P&gt;&lt;P&gt;I made an automotive product using S9KEAZN8AMFK.&lt;BR /&gt;I know that S9KEAZN8AMFK is AEC-Q100 Grade 1.&lt;BR /&gt;And the company we supply products to says they need an AEC-Q100 Grade 1 certification test report.&lt;BR /&gt;I must submit proof that S9KEAZN8AMFK is AEC-Q100 Grade 1.&lt;/P&gt;&lt;P&gt;Can you send me the AEC-Q100 Grade 1 certification test report?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;romeo&lt;/P&gt;</description>
      <pubDate>Mon, 18 Sep 2023 07:07:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S9KEAZN8AMFK-Exposed-Pad-Connection-Problems/m-p/1724514#M65549</guid>
      <dc:creator>Romeo</dc:creator>
      <dc:date>2023-09-18T07:07:22Z</dc:date>
    </item>
  </channel>
</rss>