<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K60N512 (Problems with first steps)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Problems-with-first-steps/m-p/210466#M3438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You'll need to use IAR 6.10 or later. Earlier versions of IAR don't have support for OSJTAG, which is the built-in debugger on the tower boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could alternatively use a JLink to program the board (which is supported in IAR 5.50), but you'd have to re-configure the project settings since opening the IAR 6.10 projects in IAR 5.50 corrupts the settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jun 2011 07:40:54 GMT</pubDate>
    <dc:creator>anthony_huereca</dc:creator>
    <dc:date>2011-06-02T07:40:54Z</dc:date>
    <item>
      <title>TWR-K60N512 (Problems with first steps)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Problems-with-first-steps/m-p/210465#M3437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have bought﻿&amp;nbsp;TWR-K60N512﻿. I also have installed:&lt;/P&gt;&lt;P&gt;1)IAR 5.50.6&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;2)MQX 3.7 and kwickStik_Patch&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I have problems at 4'th point of "Quick start﻿":&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have found "build_libs.eww﻿" and done everything with it. But when I had opened "TWR-K60N512_Quick_Start_Demo.eww﻿" with IAR, it wrote:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)The project 'TWR-K60N512_Quick_Start_Demo' contaains the unknown tool 'PEMICRO_ID'&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;2)Invalid driver (/driver) option&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;3) Invalid processor (/proc) option&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;4)No kernel to load&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;5)An error occured trying ti initialize the debugger. Debugging will not be available in this session&amp;nbsp;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What should﻿&amp;nbsp;I do﻿?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 May 2011 20:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Problems-with-first-steps/m-p/210465#M3437</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2011-05-28T20:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60N512 (Problems with first steps)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Problems-with-first-steps/m-p/210466#M3438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You'll need to use IAR 6.10 or later. Earlier versions of IAR don't have support for OSJTAG, which is the built-in debugger on the tower boards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could alternatively use a JLink to program the board (which is supported in IAR 5.50), but you'd have to re-configure the project settings since opening the IAR 6.10 projects in IAR 5.50 corrupts the settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2011 07:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-Problems-with-first-steps/m-p/210466#M3438</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2011-06-02T07:40:54Z</dc:date>
    </item>
  </channel>
</rss>