<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM K66 pin multiplexing</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66-pin-multiplexing/m-p/579747#M34373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Doru,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;different pins have a set list of possible alternative functions that you can mux it to. If a function is not apart of the possible pin assignments, then you can't use that function on that particular pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you look in K66's signal multiplexing and pin assignments table found in the reference manual or datasheet, you'll see that specifically PTD12 and PTD13 aren't able to serve as ADC0_SE8 or ADC1_SE8 in any of the multiplexing alternative function possibilities.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36521iB84C7D4C2E2EC003/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, as you noted in your post, PTB0 and PTB1 by default serve as ADC0_SE8 or ADC1_SE8. You may consider just using PTB0 and PTB1 instead of PTD12 and PTD13.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36759iFE0F53D3A7357710/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also, to change the functionality of a pin all you need to do is look in the PORTx_PCRn register and write appropriately to the [MUX] field.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jul 2016 15:19:25 GMT</pubDate>
    <dc:creator>charlesasquith</dc:creator>
    <dc:date>2016-07-18T15:19:25Z</dc:date>
    <item>
      <title>FRDM K66 pin multiplexing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66-pin-multiplexing/m-p/579746#M34372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guys,&lt;/P&gt;&lt;P&gt;I am trying to use ADC0_SE8 and ADC1_SE8 as adc inputs,and they are mapped to PTB0 and LLWU_P5 .How could I multiplex these signals to,for example,PTD12 and PTD13 ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 11:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66-pin-multiplexing/m-p/579746#M34372</guid>
      <dc:creator>doruirimescu</dc:creator>
      <dc:date>2016-07-18T11:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K66 pin multiplexing</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66-pin-multiplexing/m-p/579747#M34373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Doru,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;different pins have a set list of possible alternative functions that you can mux it to. If a function is not apart of the possible pin assignments, then you can't use that function on that particular pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you look in K66's signal multiplexing and pin assignments table found in the reference manual or datasheet, you'll see that specifically PTD12 and PTD13 aren't able to serve as ADC0_SE8 or ADC1_SE8 in any of the multiplexing alternative function possibilities.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36521iB84C7D4C2E2EC003/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, as you noted in your post, PTB0 and PTB1 by default serve as ADC0_SE8 or ADC1_SE8. You may consider just using PTB0 and PTB1 instead of PTD12 and PTD13.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36759iFE0F53D3A7357710/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Also, to change the functionality of a pin all you need to do is look in the PORTx_PCRn register and write appropriately to the [MUX] field.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 15:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K66-pin-multiplexing/m-p/579747#M34373</guid>
      <dc:creator>charlesasquith</dc:creator>
      <dc:date>2016-07-18T15:19:25Z</dc:date>
    </item>
  </channel>
</rss>