<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: j-link</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/j-link/m-p/578685#M34344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer attached doc file to use J-Link tool do run unlock script with your KL02 chip.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 08:21:24 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-07-19T08:21:24Z</dc:date>
    <item>
      <title>j-link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/j-link/m-p/578684#M34343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a custom board, based on the FRDM-KL02Z but with an MKL02Z16xxx instead of an MKL02Z32xxx. For programming and debugging, I am using a J-link which is is both cases directly connected to the target CPU via Vcc, GND, SWD and SWCLK (no reset). Compiler is a Keil.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the FRDM, everything works fine, I can program and debug the target CPU.&lt;/P&gt;&lt;P&gt;For the custom board, I had to change settings in the programmer but they are all now set for a see a MKL02Z32xxx. &lt;/P&gt;&lt;P&gt;However, I see a strange behavior:&amp;nbsp; Using the IDE, I always get the message that the CPU can't be reset.&lt;/P&gt;&lt;P&gt;On the other hand, if I reset and erase the CPU via the J-link commander, everything seems to be ok (but still fails sometimes).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;================================= IDE MESSAGE===================&lt;/P&gt;&lt;P&gt;------------&lt;/P&gt;&lt;P&gt;DLL: V5.12e, compiled Apr 29 2016 15:03:58&lt;/P&gt;&lt;P&gt;Firmware: J-Link V9 compiled Mar 29 2016 18:46:37&lt;/P&gt;&lt;P&gt;Hardware: V9.30&lt;/P&gt;&lt;P&gt;S/N : 269304598 &lt;/P&gt;&lt;P&gt;OEM : SEGGER-EDU &lt;/P&gt;&lt;P&gt;Feature(s) : FlashBP, GDB &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* JLink Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;&lt;P&gt;* JLink Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;&lt;P&gt;* JLink Info: Found Cortex-M0 r0p0, Little endian.&lt;/P&gt;&lt;P&gt;* JLink Info: FPUnit: 2 code (BP) slots and 0 literal slots&lt;/P&gt;&lt;P&gt;* JLink Info: CoreSight components:&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 0 @ F0002000&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 0 [0]: FFFFE000, CID: B105900D, PID: 000BB932 MTB-M0+&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 0 [1]: FFFFF000, CID: B105900D, PID: 0008E000 MTBDWT&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 0 [2]: F00FD000, CID: B105100D, PID: 000BB4C0 ROM Table&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 1 @ E00FF000&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 1 [0]: FFF0F000, CID: B105E00D, PID: 000BB008 SCS&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 1 [1]: FFF02000, CID: B105E00D, PID: 000BB00A DWT&lt;/P&gt;&lt;P&gt;* JLink Info: ROMTbl 1 [2]: FFF03000, CID: B105E00D, PID: 000BB00B FPB&lt;/P&gt;&lt;P&gt;ROMTableAddr = 0xF0002000&lt;/P&gt;&lt;P&gt;* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.&lt;/P&gt;&lt;P&gt;* JLink Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;&lt;P&gt;**JLink Warning: Failed to reset CPU. VECTRESET has confused core.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU did not halt after reset.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU could not be halted&lt;/P&gt;&lt;P&gt;* JLink Info: Core did not halt after reset, trying to disable WDT.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU did not halt after reset.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU could not be halted&lt;/P&gt;&lt;P&gt;**JLink Warning: Could not set S_RESET_ST&lt;/P&gt;&lt;P&gt;* JLink Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;&lt;P&gt;* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.&lt;/P&gt;&lt;P&gt;* JLink Info: Found SWD-DP with ID 0x0BC11477&lt;/P&gt;&lt;P&gt;**JLink Warning: Failed to reset CPU. VECTRESET has confused core.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU did not halt after reset.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU could not be halted&lt;/P&gt;&lt;P&gt;* JLink Info: Core did not halt after reset, trying to disable WDT.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU did not halt after reset.&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU could not be halted&lt;/P&gt;&lt;P&gt;**JLink Warning: Could not set S_RESET_ST&lt;/P&gt;&lt;P&gt;***JLink Error: DAP error while reading AIRCR / CPUID register&lt;/P&gt;&lt;P&gt;**JLink Warning: CPU could not be halted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Target info:&lt;/P&gt;&lt;P&gt;------------&lt;/P&gt;&lt;P&gt;Device: MKL02Z16xxx4&lt;/P&gt;&lt;P&gt;VTarget = 3.029V&lt;/P&gt;&lt;P&gt;State of Pins: &lt;/P&gt;&lt;P&gt;TCK: 0, TDI: 0, TDO: 0, TMS: 1, TRES: 1, TRST: 0&lt;/P&gt;&lt;P&gt;Hardware-Breakpoints: 0&lt;/P&gt;&lt;P&gt;Software-Breakpoints: 8192&lt;/P&gt;&lt;P&gt;Watchpoints:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;JTAG speed: 500 kHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Full Chip Erase Failed!&lt;/P&gt;&lt;P&gt;Flash Erase finished 12:35:03&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 01:04:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/j-link/m-p/578684#M34343</guid>
      <dc:creator>timjones22</dc:creator>
      <dc:date>2016-07-18T01:04:05Z</dc:date>
    </item>
    <item>
      <title>Re: j-link</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/j-link/m-p/578685#M34344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer attached doc file to use J-Link tool do run unlock script with your KL02 chip.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 08:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/j-link/m-p/578685#M34344</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-07-19T08:21:24Z</dc:date>
    </item>
  </channel>
</rss>