<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: ADC DMA Reading</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576468#M34252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC0 Status and Control Registers 1 (ADC0_SC1n) has two registers: ADC0_SC1A and ADC0_SC1B.&lt;/P&gt;&lt;P&gt;The ADC0_SC1A supports both software and hardware trigger; while the ADC0_SC1B only supports the hardware trigger.&lt;/P&gt;&lt;P&gt;Please check your below code is written value to ADC0_SC1A or ADC0_SC1B register.&lt;/P&gt;&lt;P&gt;ADC0_SC1(1)&amp;nbsp; = 0X16; &lt;/P&gt;&lt;P&gt;If write value to ADC0_SC1A, the ADC result located at ADC0_RA register;&lt;/P&gt;&lt;P&gt;While if write value to ADC0_SC1B, after hardware trigger, the ADC conversion value located at ADC0_RB register.&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 06:34:59 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-07-19T06:34:59Z</dc:date>
    <item>
      <title>ADC DMA Reading</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576467#M34251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have K60 Tower board: MK60FN1M0VLQ12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had one channel DMA read working:&lt;/P&gt;&lt;P&gt;Data result is in the register: ADC0_RA&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;ADC0_SC1(0)= 0x10;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt; // select channel 0x10&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;If I add another channel:&lt;/P&gt;&lt;P&gt; ADC0_SC1(0)= 0x10;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // select channel 0x10&lt;/P&gt;&lt;P&gt; ADC0_SC1(1)= 0x16;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // select channel 0x16&lt;/P&gt;&lt;P&gt;where is the data results:&amp;nbsp; for the channel 0x16 as above added second channel&lt;/P&gt;&lt;P&gt;is still in ADC0_RA register or in ADC0_RB ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;David Zhou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 21:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576467#M34251</guid>
      <dc:creator>davidzhou</dc:creator>
      <dc:date>2016-07-15T21:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DMA Reading</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576468#M34252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC0 Status and Control Registers 1 (ADC0_SC1n) has two registers: ADC0_SC1A and ADC0_SC1B.&lt;/P&gt;&lt;P&gt;The ADC0_SC1A supports both software and hardware trigger; while the ADC0_SC1B only supports the hardware trigger.&lt;/P&gt;&lt;P&gt;Please check your below code is written value to ADC0_SC1A or ADC0_SC1B register.&lt;/P&gt;&lt;P&gt;ADC0_SC1(1)&amp;nbsp; = 0X16; &lt;/P&gt;&lt;P&gt;If write value to ADC0_SC1A, the ADC result located at ADC0_RA register;&lt;/P&gt;&lt;P&gt;While if write value to ADC0_SC1B, after hardware trigger, the ADC conversion value located at ADC0_RB register.&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 06:34:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576468#M34252</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-07-19T06:34:59Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DMA Reading</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576469#M34253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, Hui Ma.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David Zhou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 17:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-DMA-Reading/m-p/576469#M34253</guid>
      <dc:creator>davidzhou</dc:creator>
      <dc:date>2016-07-19T17:47:12Z</dc:date>
    </item>
  </channel>
</rss>