<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K66 UDP implementation</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573125#M34164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am new to the Nxp community and Kinetis development.I would like to make an application from which the Frdm K66F sends data via UDP (or TCP) to a computer.The support and documentation are mostly non-existent on this topic,my question is how would you go about making this happen ? Perhaps you could point me to some example or reference,if there exists such thing.&lt;/P&gt;&lt;P&gt;Best wishes :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jul 2016 12:57:59 GMT</pubDate>
    <dc:creator>doruirimescu</dc:creator>
    <dc:date>2016-07-14T12:57:59Z</dc:date>
    <item>
      <title>K66 UDP implementation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573125#M34164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I am new to the Nxp community and Kinetis development.I would like to make an application from which the Frdm K66F sends data via UDP (or TCP) to a computer.The support and documentation are mostly non-existent on this topic,my question is how would you go about making this happen ? Perhaps you could point me to some example or reference,if there exists such thing.&lt;/P&gt;&lt;P&gt;Best wishes :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 12:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573125#M34164</guid>
      <dc:creator>doruirimescu</dc:creator>
      <dc:date>2016-07-14T12:57:59Z</dc:date>
    </item>
    <item>
      <title>Re: K66 UDP implementation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573126#M34165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;​Hi Doru,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to refer to the set of lwip demos which is from the KSDK2.0, and in the set of lwip demos, it contains a TCP echo and a UDP echo demo.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329744"&gt;How to: install KSDK 2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 08:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573126#M34165</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-15T08:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: K66 UDP implementation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573127#M34166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also using K66 MCU.&lt;/P&gt;&lt;P&gt;As per your suggestion I used SDK2.0 (lwip_UDP_echo)example , Its working perfectly.&lt;/P&gt;&lt;P&gt;Now Can you help me to modify the example as per our requirement, so that it should not echo back UDP packet, instead i need simple UDP receive/ send example.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;tried by removing echo send function , but in PC side it still waiting for UDP echo packet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.,&lt;/P&gt;&lt;P&gt;karthik&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Dec 2016 08:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-UDP-implementation/m-p/573127#M34166</guid>
      <dc:creator>karthikas</dc:creator>
      <dc:date>2016-12-10T08:04:58Z</dc:date>
    </item>
  </channel>
</rss>