<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-K64: WFI used, but does not sleep</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572591#M34145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please use this code to enter your lls mode:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14685525431026812 jive_text_macro" data-renderedposition="60_8_1192_384" jivemacro_uid="_14685525431026812" modifiedtitle="true"&gt;&lt;P&gt;void enter_lls(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; volatile unsigned int dummyread;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Write to PMPROT to allow LLS power modes this write-once &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bit allows the MCU to enter the LLS low power mode*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMPROT = SMC_PMPROT_ALLS_MASK;&amp;nbsp;&amp;nbsp; //0x8u&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Set the STOPM field to 0b011 for LLS mode&amp;nbsp; */&lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMCTRL &amp;amp;= ~SMC_PMCTRL_STOPM_MASK; &lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMCTRL |=&amp;nbsp; SMC_PMCTRL_STOPM(0x3); &lt;/P&gt;&lt;P&gt;&amp;nbsp; /*wait for write to complete to SMC before stopping core */&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; dummyread = SMC_PMCTRL;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Now execute the stop instruction to go into LLS */&lt;/P&gt;&lt;P&gt;&amp;nbsp; stop();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void stop (void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SCB_SCR |= SCB_SCR_SLEEPDEEP_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* WFI instruction will start entry into STOP mode */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("WFI");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should enable the lls mode in SMC_PMPROT register, and please note, the PMPROT register can be written only once after any system reset, so you should make sure the PMPROT register has not been wrote before.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2016 03:19:04 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-07-15T03:19:04Z</dc:date>
    <item>
      <title>FRDM-K64: WFI used, but does not sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572589#M34143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to prove that I can put the K64 module on the FRDM board to LLS sleep mode, but when I execute the __asm("WFI") command, it skips over any sleep attempts and moves on to the next line of code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A brief into to my code, and the order of operation: Green LED is turned on and the wake handler is supposed to turn it off. This never happens. In fact with debugger I have seen that the asm("WFI") code is practically skipped over. An external pin is supposed to be used to trigger wake on rising edge. Any help is appreciated.&lt;/P&gt;&lt;P&gt;[code begin]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define GLED_ON (GPIOE_PDOR &amp;amp;= ~(1&amp;lt;&amp;lt; 26))&lt;/P&gt;&lt;P&gt;#define GLED_OFF (GPIOE_PDOR |= (1&amp;lt;&amp;lt;26) )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void&lt;/P&gt;&lt;P&gt;disableRTC()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;//This function is used when RTC is known to keep pending interrupt at startup...(erratta note)&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM-&amp;gt;SCGC6 |=SIM_SCGC6_RTC_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // enable clock to RTC&lt;/P&gt;&lt;P&gt;&amp;nbsp; RTC-&amp;gt;TSR = 0x00;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // dummy write to RTC TSR per errata 8068&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM-&amp;gt;SCGC6 &amp;amp;= ~SIM_SCGC6_RTC_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // disable clock to RTC&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;wakeIRQHandler()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Is only used to turn off the GREEN led on board&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sleep_init()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTC_PCR11 = 0x00090102;&amp;nbsp;&amp;nbsp;&amp;nbsp; // PTC11 Wakeup rising edge, Pull-down, rising edge reset, enable IRQ&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_PE3 = 0x40;&amp;nbsp;&amp;nbsp;&amp;nbsp; // LLWU_P11 rising edge detection&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_InstallIntHandler(LLWU_IRQn, wakeIRQHandler);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;init()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM_HAL_EnableClock(SIM,kSimClockGatePortC);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //For wake pin&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM_HAL_EnableClock(SIM,kSimClockGatePortE);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //For green led pin&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTE_PCR26 = 0x00000103;&lt;/P&gt;&lt;P&gt;&amp;nbsp; GPIOE_PDDR = (1 &amp;lt;&amp;lt; 26); // Make led-green an output&lt;/P&gt;&lt;P&gt;&amp;nbsp; GLED_ON;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Make sure green LED is on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sleep_init();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;goto_sleep()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;volatile unsigned int sync_read;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_F1 = 0xFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LLWU_F2 = 0xFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMC_PMCTRL = 0x03; // set stop mode to LLS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sync_read = SMC_PMCTRL; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sync_read++;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Silence compiler warning&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm("WFI"); //Issue wait for interrupt asm&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sync_read++;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Silence compiler warning&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;/P&gt;&lt;P&gt;&amp;nbsp; PE_low_level_init();&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*** End of Processor Expert internal initialization.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ***/&lt;/P&gt;&lt;P&gt;init();&lt;/P&gt;&lt;P&gt;goto_sleep();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while(1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//never get here&lt;/P&gt;&lt;P&gt;return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;[code end]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 20:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572589#M34143</guid>
      <dc:creator>briandwyer</dc:creator>
      <dc:date>2016-07-14T20:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64: WFI used, but does not sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572590#M34144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a correction to the IRQ handler:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;wakeIRQHandler()&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;{&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Is only used to turn off the GREEN led on board&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GLED_OFF;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;{&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 23:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572590#M34144</guid>
      <dc:creator>briandwyer</dc:creator>
      <dc:date>2016-07-14T23:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64: WFI used, but does not sleep</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572591#M34145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please use this code to enter your lls mode:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_14685525431026812 jive_text_macro" data-renderedposition="60_8_1192_384" jivemacro_uid="_14685525431026812" modifiedtitle="true"&gt;&lt;P&gt;void enter_lls(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; volatile unsigned int dummyread;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Write to PMPROT to allow LLS power modes this write-once &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bit allows the MCU to enter the LLS low power mode*/&lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMPROT = SMC_PMPROT_ALLS_MASK;&amp;nbsp;&amp;nbsp; //0x8u&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Set the STOPM field to 0b011 for LLS mode&amp;nbsp; */&lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMCTRL &amp;amp;= ~SMC_PMCTRL_STOPM_MASK; &lt;/P&gt;&lt;P&gt;&amp;nbsp; SMC_PMCTRL |=&amp;nbsp; SMC_PMCTRL_STOPM(0x3); &lt;/P&gt;&lt;P&gt;&amp;nbsp; /*wait for write to complete to SMC before stopping core */&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp; dummyread = SMC_PMCTRL;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Now execute the stop instruction to go into LLS */&lt;/P&gt;&lt;P&gt;&amp;nbsp; stop();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void stop (void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set the SLEEPDEEP bit to enable deep sleep mode (STOP) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SCB_SCR |= SCB_SCR_SLEEPDEEP_MASK;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* WFI instruction will start entry into STOP mode */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm("WFI");&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should enable the lls mode in SMC_PMPROT register, and please note, the PMPROT register can be written only once after any system reset, so you should make sure the PMPROT register has not been wrote before.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 03:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64-WFI-used-but-does-not-sleep/m-p/572591#M34145</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-07-15T03:19:04Z</dc:date>
    </item>
  </channel>
</rss>